This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AWR1843: 芯片供电及复位信号满足上电时序要求,但芯片不能正常工作

Part Number: AWR1843

TI团队,您好

          我们基于AWR1843芯片,设计了自己的雷达硬件板,电源方案采用了官方的LP87702D,在调试AWR1843芯片时,出现了有部分硬件板上电后不能正常启动工作的问题。

针对有问题的硬件板进行调试,给芯片供电的3.3V,1.8V,1.0V等电压都是正常的,用示波器测量供电及复位信号时序,也满足手册上所要求的。(nReset复位信号上升沿比VIOIN电源延后10ms左右)

但测量 WARMRESET OUTPUT信号,波形如下,信号有异常,电平电压后面一致维持在2.2V,

测量VBGAP OUTPUT输出信号,一致是低电平(0V),正常情况下应该是有1V的电平输出;

测量 40M晶振,无振荡波形输出,已经确认过匹配电容没有问题。

另外发现雷达板出现以上异常情况后,在2s内进行断电上电操作,芯片能正常启动,测试WARMRESET OUTPUT信号,VBGAP OUTPUT信号,40M晶振频率都是正常的。

所以想请教出现这种问题的具体原因是什么?复位信号的上升沿延时是否有具体要求?还是说延时大于3ms就可以?

感谢解答!

x 出现错误。请重试或与管理员联系。