This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

OPT3101: 距离精度确定

Part Number: OPT3101

你好,

    使用OPT3101官方SDK测量距离,请问我们可以通过那个输出参数评估测量距离的精度,或者说可靠度。

   谢谢!

  • 您好,是这样的,OPT3101 只是一个模拟前端AFE,或者说是一个外界光学器件的AFE,因为光学器件都是外接的,所以距离,精度视场Fov都和其他特性在很大程度上是取决于所选择的光学。我们的OPT3101EVM 视野距离为10m,视场为10度。我们有一些第三方的合作伙伴使用OPT3101将范围已经夸大到40m。链接如下,您也可以参考下。

    https://www.ti.com/tool/BW-3P-TF02-PRO