Other Parts Discussed in Thread: LDCCOILEVM, LDC1614
想继续问一下:
1.在20cm的距离上如何感应判断井盖的开关,线圈直径需要多大?
2、远距离情况下如何提高灵敏度?
3.为什么上位机软件显示通道3的常态波形是这样的,感觉变化很大,如何判断出开关特征?

This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
想继续问一下:
1.在20cm的距离上如何感应判断井盖的开关,线圈直径需要多大?
2、远距离情况下如何提高灵敏度?
3.为什么上位机软件显示通道3的常态波形是这样的,感觉变化很大,如何判断出开关特征?

您好,
为更加有效地解决您的问题,我已将您的问题发布在E2E英文技术论坛上,请更了解这款芯片的TI资深工程师为您解答:
https://e2e.ti.com/support/sensors-group/sensors/f/sensors-forum/1194680/ldc1614evm-ldc1614
您好,您可以在下面中文和英文E2E论坛上咨询问题:
中文技术论坛:https://e2echina.ti.com/
英文技术论坛:https://e2e.ti.com/
以上信息我已经反馈给E2E英文工程师,请等待他们的答复。
已得到E2E英文工程师的答复:如果没有办法将传感器线圈靠近目标,那么我认为电感传感器不是此应用的正确选择。20cm距离对于电感传感器来说是不可行的,因此需要考虑另一种解决方案。在这么远的距离里,你可以考虑超声波一类的传感器。
对于50mm,我们建议使用50mm线圈来感测目标。当目标距离达到线圈直径的100%时,它们之间的耦合将是最小的,但在此范围内仍可实现开/闭检测。为获得最佳耦合效果,目标应至少与传感器线圈的尺寸相同。有关详细信息,请参阅https://e2e.ti.com/blogs_/b/analogwire/posts/inductive-sensing-target-size-matters 帖子。
我们在LDCCOILEVM中有一个46mm线圈,可用于帮助建立原型。
电感线圈的直径大小与检测距离的关系?
感应系统的感应距离主要取决于传感器线圈的外径。大多数LDC设备最多只能感应50%的传感器线圈直径。因此更大的线圈具有更大的感应距离。请注意,目标离线圈越近,感应响应就越强。更多信息见:[FAQ] Inductive sensing FAQ - Frequently asked questions
前两个问题我已提交到E2E英文论坛,请等待E2E工程师的回复。
E2E工程师的回复:
1、我们通常建议使用与LDC设备叠层的平面线圈。对于类似的平面线圈和叠层线圈之间的检测距离,我们没有任何直接比较。
2、决定检测距离的主要因素是传感器线圈的外径。在某些情况下,改变电感/电容会产生较小的影响,但影响不如改变传感器线圈直径大。
Can you share any diagram/drawing of the coil and the nearby metal that you are trying to shield from?
您可以分享线圈和您试图屏蔽的附近金属的图纸吗?我想这里他应该需要他们的形状和相对位置图