This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AWR2243: 4芯片级联环境下不同monitoring chirp的slope配置下,移相器监控到的各Tx的相位不同

Part Number: AWR2243


您好,

我在4个AWR2243级联环境下,统计了两组移相器监控报告数据,发现不同monitoring chirp slope配置条件下,统计的4个芯片共12个移相器的相位存在差异,为什么会存在差异呢?原本理解移相器的相位偏差是由于制造误差 和硬件本身特性决定,为什么测量结果会受monitoring chirp slope变化影响呢?

通过AWR_MONITOR_TX0_PHASE_SHIFTER_CONF_SB、AWR_MONITOR_TX1_PHASE_SHIFTER_CONF_SB、AWR_MONITOR_TX2_PHASE_SHIFTER_CONF_SB配置同样的PROFILE_INDX,其中开始频率为79GHz,PH_SHIFTER_MON_CFG为3,PH_SHIFTER_INC_VAL1为0,PH_SHIFTER_INC_VAL2为4,PH_SHIFTER_MON1和PH_SHIFTER_MON2均为0,两次统计分别配置不同的MON_CHIRP_SLOPE,一组为7,一组为28。

通过统计AWR_MONITOR_TX0_PHASE_SHIFTER_REPORT_AE_SB、AWR_MONITOR_TX1_PHASE_SHIFTER_REPORT_AE_SB、AWR_MONITOR_TX2_PHASE_SHIFTER_REPORT_AE_SB中的PH_SHIFTER_MON_VAL1和PH_SHIFTER_MON_VAL2发现,两次统计的同一芯片同一Tx的PH_SHIFTER_MON_VAL1存在差异,偏差5~10°,并且计算出的各FTTI下移相偏差变化也不一致。

预期的结果应该是同一芯片同一Tx的PH_SHIFTER_MON_VAL1基本一致,移相偏差随FTTI的变化也基本一致。