This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRV411: 参数问题

Part Number: DRV411


1.数据表中说可以有效消除霍尔原件的偏移和漂移 ,是否代表可以消除霍尔的温漂?

2.数据表中可以提供250mA H桥驱动传感器补偿线圈 ,这个是否与量程强相关?如果是,设计时通过增加线圈匝数,是否能达到提升量程的效果?如果线圈电阻过大,是否会导致DRV411提前饱和?

3.对于磁芯的材质是否有特殊要求?有无推荐材料

4、error的信息包含哪些?是否可以分享在客户端的error报错的案例?

  • 您好,

    1、是的

    2、是的,根据其工作原理,补偿线圈的驱动电流越大,在同样补偿线圈匝数时,可以测量的电流范围越大。

    是的,我认为可以考虑通过增加补偿线圈匝数来扩大测量量程。

    是的,要考虑线圈电阻+shunt电阻,在驱动电流下其电压摆幅的限制:

    3、有许多不同的材料可用于磁芯。需根据材料性能、电流测量范围要求以及所需的机械形状和成本等标准来确定选择。下面文档的 第2部分 Core and Hall Sensor Considerations 有一些相关说明:

    Design Considerations for the DRV411

    4、下面datasheet 截图说明了 error flag的条件:

    下面参考设计希望对您有帮助:

    https://www.ti.com/tool/TIPD184