This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

OPT3001: 传感器的线性度是如何计算的?

Part Number: OPT3001


当<40lux input时,线性度5%;>40 lux input时,线性度2%。 

是否可以理解为,如果当环境光照度5000lux,ALS读数偏差为5000lux*2%=100 lux?

  • 您好,

    线性度是指实际输出、输入的关系曲线和理想关系曲线之间的最大偏差与满量程的百分比。这个是指关系曲线中的最大误差百分比,并不是指每一个输出都有这么大的误差。