This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMP91000: 跨阻放大器的使用问题

Part Number: LMP91000


您好:

我使用三电极模式进行电化学测试,数据手册显示TIA的放大倍数等于RTIA,我改变TIACN寄存器使RTIA分别对应于3.5kΩ、35kΩ和350kΩ,Vout连接MCU的ADC,得到的的结果应该分别相差10倍的关系,但实际上并没有,我在同一时间做的实验,输入电流可以看作相等,3.5kΩ、35kΩ和350kΩ对应的转换的结果分别是40mV、2mV和100mV。我想知道这是为什么,我希望将电流放大得更大,谢谢工程师的帮助!

这是我的电路图