我在使用studio配置雷达chirp数量时,设置参数为256,运行lua后就会报错,显示超过最大值,尝试255就可以。最大只能设置255的chirp数量是否太少了一些。

This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
我在使用studio配置雷达chirp数量时,设置参数为256,运行lua后就会报错,显示超过最大值,尝试255就可以。最大只能设置255的chirp数量是否太少了一些。

您可以看一下高级帧的配置。
6 Advanced Chirp Configurations
https://www.ti.com/lit/an/swra553a/swra553a.pdf
To provide maximum flexibility of the chirps within a frame the advanced frame config API provides the ability to break a frame into different sub frames (up to 4). Each of the sub frames consists of multiple bursts of chirps (up to 512 bursts) .
HI Nancy,
请问这个高级帧配置有没有参考配置看一下呢?
BR
以下帖子中有讨论,参考看一下:
13. Advanced Frame Config Tab operations