Part Number: AWR1843BOOST
你好,我在TI的demo中尝试启动HWA,但是却发现有问题,我的初始化步骤如下
1.对照C:\ti\mmwave_sdk_03_03_00_03\mmwave_sdk_03_03_00_03\packages\ti\drivers\hwa\test\common中main.c中的文件,首先添加所有的头文件
* Standard Include Files. */ #include <stdint.h> #include <stdlib.h> #include <stddef.h> #include <string.h> #include <stdio.h> /* BIOS/XDC Include Files. */ #include <xdc/std.h> #include <xdc/cfg/global.h> #include <xdc/runtime/IHeap.h> #include <xdc/runtime/System.h> #include <xdc/runtime/Error.h> #include <xdc/runtime/Memory.h> #include <ti/sysbios/BIOS.h> #include <ti/sysbios/knl/Task.h> #include <ti/sysbios/knl/Event.h> #include <ti/sysbios/knl/Semaphore.h> #include <ti/sysbios/knl/Clock.h> #include <ti/sysbios/heaps/HeapBuf.h> #include <ti/sysbios/heaps/HeapMem.h> #include <ti/sysbios/knl/Event.h> /* mmWave SK Include Files: */ #include <ti/common/sys_common.h> #include <ti/drivers/osal/SemaphoreP.h> #include <ti/drivers/esm/esm.h> #include <ti/drivers/hwa/hwa.h> #include <ti/drivers/soc/soc.h> #include <ti/utils/testlogger/logger.h>
2.在dss端的main.c中初始化一个进程
/* Initialize the SOC Module: This is done as soon as the application is started
* to ensure that the MPU is correctly configured. */
gSOCHandle = SOC_init (&socCfg, &errCode);
if (gSOCHandle == NULL)
{
System_printf ("Error: SOC Module Initialization failed [Error code %d]\n", errCode);
return -1;
}
/* Initialize test logger */
// MCPI_Initialize();
/* Initialize the Task Parameters. */
Task_Params_init(&taskParams);
taskParams.stackSize = 4*1024;
Task_create(Test_initTask, &taskParams, NULL);
3.该进程的的初始化函数内容为
static void Test_initTask(UArg arg0, UArg arg1)
{
HWA_Handle handle;
int32_t errCode, compareCode1, compareCode2;
uint8_t paramsetIdx = 0, pingParamSetIdx = 0;// pongParamSetIdx = 0;
uint8_t *srcAddr = (uint8_t*)SOC_HWA_MEM0;
uint8_t *dstAddr = (uint8_t*)SOC_HWA_MEM2;
#ifdef TEST_PARAMSET_INTERRUPT
HWA_InterruptConfig paramISRConfig;
SemaphoreP_Handle paramSetSem;
#endif
SemaphoreP_Handle doneSem;
SemaphoreP_Params semParams;
SemaphoreP_Status status;
/**************************************************************************
* Initialize the HWA
**************************************************************************/
HWA_init();
// MCPI_setFeatureTestResult("API HWA_init()", MCPI_TestResult_PASS);
/* Debug Message: */
System_printf ("Debug: HWA has been initialized\n");
}
完成上述操作之后,我尝试debug该程序,给出的系统日志如下

我想请问可能是哪方面的原因呢?
谢谢!