This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AWR1843BOOST: 和DCA1000EVM一块使用,在mmwave studio中SPI connectivity 一直连接不成功

Part Number: AWR1843BOOST
Other Parts Discussed in Thread: DCA1000EVM

是这样的,我购买了两块awr1843boost开发板,和一块DCA1000EVM用来采集数据,但我使用一块awr开发版与DCA1000时,在mmwave studio软件中一直显示spi,连接不成功,我采用上官网上说的擦除flash,S2开关也拉置spi处,但是一直不成功,之后我选择了备用板和dca1000一起操作,在mmwave studio中,与之前操作流程一致,这一套显示spi连接成功,请问一下这是什么原因造成的呢?

  • 请问供电电压是板子5-V, > 2.5-A吗?两块板子是一起买的吗?能否把log信息发一下?

  • 是一块买的,log信息是指什么呢?两块板子都是给的5v,2A,一块板子可以正常用,一块不可以连接spi

  • 连接不上的那个板子之前我经过多次擦除,请问这个有影响吗?

  • 请问问题解决了吗?我看到您确认答案了。

    连接不上的那个板子之前我经过多次擦除,请问这个有影响吗?

    这个应该不会有影响。

    两块板子都是给的5v,2A

    请尝试把用2.5A以上的电源供电。

  • GM: Constructor
    GM: Fri Mar 31 15:45:48 2023
    RSTD.Transmit("/Settings")
    [15:45:49]
    [15:45:49] ### Running Startup script: "C:\TI\mmwave_studio_02_01_01_00\mmWaveStudio\Scripts\Startup.lua" ###
    [15:45:49] RSTD.SetAndTransmit ("/Settings/Scripter/Display DateTime" , "1")
    [15:45:49] RSTD.SetAndTransmit ("/Settings/Scripter/DateTime Format" , "HH:mm:ss")
    [15:45:49] Scripter ignored: Attempt to UnBuild() again or before Build.
    [15:45:49] RSTD.SetVar ("/Settings/Clients/Client 0/Dll" , "C:\\TI\\mmwave_studio_02_01_01_00\\mmWaveStudio\\Clients\\\\LabClient.dll")
    [15:45:49] RSTD.SetVar ("/Settings/Clients/Client 0/Use" , "TRUE")
    [15:45:49] RSTD.SetVar ("/Settings/Clients/Client 1/Use" , "FALSE")
    [15:45:49] RSTD.SetVar ("/Settings/Clients/Client 2/Use" , "FALSE")
    [15:45:49] RSTD.SetVar ("/Settings/Clients/Client 3/Use" , "FALSE")
    [15:45:49] RSTD.SetVar ("/Settings/Clients/Client 4/Use" , "FALSE")
    [15:45:49] RSTD.SetVar ("/Settings/AL Client/AL Dll" , "C:\\TI\\mmwave_studio_02_01_01_00\\mmWaveStudio\\RunTime\\SAL.dll")
    [15:45:49] RSTD.SetVar ("/Settings/Clients/Client 0/GuiDll" , "")
    [15:45:49] RSTD.SetVar ("/Settings/AutoUpdate/Enabled" , "TRUE")
    [15:45:49] RSTD.SetVar ("/Settings/AutoUpdate/Interval" , "1")
    [15:45:49] RSTD.SetVar ("/Settings/Monitors/UpdateDisplay" , "TRUE")
    [15:45:49] RSTD.SetVar ("/Settings/Monitors/OneClickStart" , "TRUE")
    [15:45:49] RSTD.SetVar ("/Settings/Automation/Automation Mode" , "false")
    [15:45:49] RSTD.Transmit("/")
    [15:45:49] RSTD.SaveSettings(): Settings saved to "C:\Users\Administrator\AppData\Roaming\RSTD\config.xml"
    [15:45:49] RSTD.Build()
    [15:45:49] RSTD.SaveSettings(): Settings saved to "C:\Users\Administrator\AppData\Roaming\RSTD\config.xml"
    [15:45:49] RSTD.Transmit("/")
    [15:45:49] RSTD.AL_Build()
    [15:45:49] RSTD.AL_LoadXml()
    [15:45:49] RSTD.Transmit("/")
    [15:45:49] RSTD.AL_Init()
    [15:45:49] RSTD.Clients_Build()
    [15:45:49] GM: Init
    [15:45:49] GM: Loaded 'C:\TI\mmwave_studio_02_01_01_00\mmWaveStudio\Clients\\LabClient.dll'
    [15:45:49] GM: 1 Guest (s) init
    [15:45:49] GM: 1 Module(s) init
    [15:45:49] GM: 2 Tab (s) init
    [15:45:49] RSTD.Client_LoadXml()
    [15:45:49] [RadarAPI]: ar1.selectRadarMode(0)
    [15:45:49] [RadarAPI]: Status: Passed
    [15:45:49] Matlab Runtime Engine is installed
    [15:45:49] [RadarAPI]: Starting Matlab Engine..
    [15:45:58] [RadarAPI]: Matlab Engine Started!
    [15:46:00] [RadarAPI]: ar1.selectCascadeMode(0)
    [15:46:00] [RadarAPI]: Status: Passed
    [15:46:00] [RadarAPI]: ar1.LoadSettings('C:\Users\Administrator\AppData\Roaming\RSTD\ar1gui.ini')
    [15:46:00] TESTING = false
    [15:46:00] RstdNet: Port 2777: Listening..
    [15:46:00]
    [15:46:00] ***Script completed successfully.***
    [15:46:25] [RadarAPI]: Opening Gpio Control Port()
    [15:46:25] Status: Failed to open/close GpioControl, Error Type: PROTOCOL ERROR
    [15:46:25] [RadarAPI]: Opening Board Control Port()
    [15:46:25] [RadarAPI]: Status: Failed to open/close BoardControl, Error value: -1
    [15:46:26] [RadarAPI]: ar1.FullReset()
    [15:46:26] [RadarAPI]: Status: Failed To give full reset, Error Value: -7
    [15:46:27] [RadarAPI]: ar1.SOPControl(2)
    [15:46:27] [RadarAPI]: Status: Passed
    [15:46:42] [RadarAPI]: ar1.Connect(5,115200,1000)
    [15:46:43] [RadarAPI]: ar1.Calling_IsConnected()
    [15:46:44] [RadarAPI]: ar1.SelectChipVersion("AR1642")
    [15:46:44] [RadarAPI]: Status: Passed
    [15:46:44] [RadarAPI]: ar1.SelectChipVersion("AR1642")
    [15:46:44] [RadarAPI]: Status: Passed
    [15:46:44] [RadarAPI]: ar1.deviceVariantSelection("XWR1843")
    [15:46:44] [RadarAPI]: Status: Passed
    [15:46:44] [RadarAPI]: ar1.frequencyBandSelection("77G")
    [15:46:44] [RadarAPI]: ar1.SelectChipVersion("XWR1843")
    [15:46:44] [RadarAPI]: Status: Passed
    [15:46:44] Device Status : XWR1843/ASIL-B/SOP:2/ES:2
    [15:46:44] [RadarAPI]: ar1.SaveSettings('C:\Users\Administrator\AppData\Roaming\RSTD\ar1gui.ini')
    [15:46:47] [RadarAPI]: ar1.DownloadBSSFw("C:\\TI\\mmwave_studio_02_01_01_00\\mmWaveStudio\\Scripts\\..\\..\\rf_eval_firmware\\radarss\\xwr18xx_radarss.bin")
    [15:46:48] [RadarAPI]: Downloading BSS Patch RPRC Binary..
    [15:46:55] [RadarAPI]: ar1.GetBSSFwVersion()
    [15:46:55] [RadarAPI]: BSSFwVersion:(02.00.00.01 (05/10/17))
    [15:46:56] [RadarAPI]: ar1.GetBSSPatchFwVersion()
    [15:46:56] [RadarAPI]: BSSPatchFwVersion:(01.02.05.02 (30/04/19))
    [15:46:58] [RadarAPI]: ar1.DownloadMSSFw("C:\\TI\\mmwave_studio_02_01_01_00\\rf_eval_firmware\\masterss\\xwr18xx_masterss.bin")
    [15:46:58] [RadarAPI]: Downloading MSS RPRC Binary..
    [15:47:09] [RadarAPI]: ar1.GetMSSFwVersion()
    [15:47:09] [RadarAPI]: MSSFwVersion:(01.02.05.02 (16/07/19))
    [15:47:13] [RadarAPI]: ar1.PowerOn(0, 1000, 0, 0)
    [15:47:13] Status: Failed, Error Type: RADAR INTERFACE ERROR
    [15:47:18] MSS Power Up async event was not received!

  • 有可能是板子硬件的问题,请按照以下方式联系客户支持部门的技术部门,会有技术客服为您提供帮助。

    • 打开链接https://ticsc.service-now.com/csm
    • 点击申请新的支持下面的提交申请按钮
    • 在新打开的窗口中点击技术帮助下面的创建案例按钮
    • 在打开的表格中您可以使用中文描述您的问题并且递交。递交申请时,请您提及以下信息:
      • Ti.com购买订单号
      • 需要技术鉴定EVM是否存在质量问题
      • 您是否使用免费邮箱注册myti账号