Part Number: AWR1843BOOST
Other Parts Discussed in Thread: AWR1843
你好,
我使用的是开发板是AWR1843,我是用的demo是AutomotiveToolbox\mmwave_industrial_toolbox_4_1_0\labs\level_sensing\16xx_high_accuracy以此为基础的18xx版本的测距demo,这个demo由一个叫chris meng的工程师给出
原始参数为:
dfeDataOutputMode 1
channelCfg 1 1 0
adcCfg 2 1
adcbufCfg 0 1 1 1
profileCfg 0 77 7 7 114.4 0 0 33.71 1 512 5000 0 0 48
chirpCfg 0 0 0 0 0 0 0 1
frameCfg 0 0 10 0 500 1 0
lowPower 0 0
guiMonitor 1 1 0 0 0 1
RangeLimitCfg 2 1 1.0 3.0
sensorStart
我想修改为:
dfeDataOutputMode 1
channelCfg 1 1 0
adcCfg 2 1
adcbufCfg 0 1 1 1
profileCfg 0 77 5 7 45 0 0 80 1 64 2000 0 0 48
chirpCfg 0 0 0 0 0 0 0 1
frameCfg 0 0 10 0 500 1 0
lowPower 0 0
guiMonitor 1 1 0 0 0 1
RangeLimitCfg 2 1 1.0 3.0
sensorStart
我主要更改了profileCfg这个参数,然后我通过串口发送配置,consolo报错如下:
********************************************** Debug: MMWDemoMSS Launched the Initialization Task Debug: MMWDemoMSS mmWave Control Initialization was successful Debug: CLI is operational [C674X_0] Debug: MMWDemoDSS ADCBUF Instance(0) @008095d0 has been opened successfully Debug: MMWDemoDSS Data Path init succeeded Debug: MMWDemoDSS initTask exit [Cortex_R4_0] numRangeBinZoomIn=2,left=0,right=0 enableRangeLimit=1,skipMin=1.000000,skipMax=3.000000 Debug: MMWDemoMSS Received CLI sensorStart Event Debug: System Heap (TCM): Size: 65536, Used = 33376, Free = 32160 bytes Debug: MMWDemoMSS mmWave config succeeded [C674X_0] DSS:enableRangeLimit=1,skipMin=1.00,skipMax=3.00,rangeResolution=0.0586,skipLeft=17,skipRight=13 DDR Heap : size 65536 (0x10000), used 8248 (0x2038) LL2 Heap : size 20480 (0x5000), used 2236 (0x8bc) LL2 Scratch : size 8192 (0x2000), used 1024 (0x400) LL1 Scratch : size 16384 (0x4000), used 4096 (0x1000) HSRAM Heap : size 8192 (0x2000), used 0 (0x0) [Cortex_R4_0] Debug: MMWDemoMSS Received CLI sensorStart Event Error: MMWDemoMSS mmWave Configuration failed [Error code -203816626] Debug: MMWDemoMSS Received CLI sensorStart Event Error: MMWDemoMSS mmWave Configuration failed [Error code -203816626]
我想知道,这个报错我改去修改那一部分,或者参照什么可以解决这个问题。
谢谢