您好,我尝试使用powershell和cmd运行Automation.lua,但mmwavestudio只是执行到connecton,就不会向下执行了。所以,我未采集到任何的数据。

mmwavestudio输出以下错误提示:

我不知是为何?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好,我尝试使用powershell和cmd运行Automation.lua,但mmwavestudio只是执行到connecton,就不会向下执行了。所以,我未采集到任何的数据。

mmwavestudio输出以下错误提示:

我不知是为何?
请看一下直接在mmwave studio里执行lua可以吗?
8. Select the DataCapturedemo_xWR.lua file from the \mmwaveStudio\Scripts\ folder by clicking on the browse button, then click on the run button.
https://www.ti.com/lit/ml/spruik7/spruik7.pdf
请问matlab是否安装mmwave studio user guide里的版本?
Install 32-bit Matlab Runtime Engine (Version 8.5.1): It is used to run the PostProcessing utility within mmWaveStudio. in.mathworks.com/.../R2015 aSP1/installers/win32/MCR_R2015aSP1_win32_installer.exe
请问电脑操作系统是win7或者win10。我这边试了一下。
GM: Constructor
GM: Thu Apr 06 14:39:50 2023
RSTD.Transmit("/Settings")
[14:39:50]
[14:39:50] ### Running Startup script: "C:\ti\mmwave_studio_02_01_01_00\mmWaveStudio\Scripts\Startup.lua" ###
[14:39:50] Can't run "C:\ti\mmwave_studio_02_01_01_00\mmWaveStudio\Scripts\Startup.lua" since another Lua operation is in process.
[14:39:50] RSTD.SetAndTransmit ("/Settings/Scripter/Display DateTime" , "1")
[14:39:50] RSTD.SetAndTransmit ("/Settings/Scripter/DateTime Format" , "HH:mm:ss")
[14:39:50] Scripter ignored: Attempt to UnBuild() again or before Build.
[14:39:50] RSTD.SetVar ("/Settings/Clients/Client 0/Dll" , "C:\\ti\\mmwave_studio_02_01_01_00\\mmWaveStudio\\Clients\\\\LabClient.dll")
[14:39:50] RSTD.SetVar ("/Settings/Clients/Client 0/Use" , "TRUE")
[14:39:50] RSTD.SetVar ("/Settings/Clients/Client 1/Use" , "FALSE")
[14:39:50] RSTD.SetVar ("/Settings/Clients/Client 2/Use" , "FALSE")
[14:39:50] RSTD.SetVar ("/Settings/Clients/Client 3/Use" , "FALSE")
[14:39:50] RSTD.SetVar ("/Settings/Clients/Client 4/Use" , "FALSE")
[14:39:50] RSTD.SetVar ("/Settings/AL Client/AL Dll" , "C:\\ti\\mmwave_studio_02_01_01_00\\mmWaveStudio\\RunTime\\SAL.dll")
[14:39:50] RSTD.SetVar ("/Settings/Clients/Client 0/GuiDll" , "")
[14:39:50] RSTD.SetVar ("/Settings/AutoUpdate/Enabled" , "TRUE")
[14:39:50] RSTD.SetVar ("/Settings/AutoUpdate/Interval" , "1")
[14:39:50] RSTD.SetVar ("/Settings/Monitors/UpdateDisplay" , "TRUE")
[14:39:50] RSTD.SetVar ("/Settings/Monitors/OneClickStart" , "TRUE")
[14:39:50] RSTD.SetVar ("/Settings/Automation/Automation Mode" , "false")
[14:39:50] RSTD.Transmit("/")
[14:39:50] RSTD.SaveSettings(): Settings saved to "C:\Users\\AppData\Roaming\RSTD\config.xml"
[14:39:50] RSTD.Build()
[14:39:51] RSTD.SaveSettings(): Settings saved to "C:\Users\\AppData\Roaming\RSTD\config.xml"
[14:39:51] RSTD.Transmit("/")
[14:39:51] RSTD.AL_Build()
[14:39:51] RSTD.AL_LoadXml()
[14:39:51] RSTD.Transmit("/")
[14:39:51] RSTD.AL_Init()
[14:39:51] RSTD.Clients_Build()
[14:39:51] GM: Init
[14:39:51] GM: Loaded 'C:\ti\mmwave_studio_02_01_01_00\mmWaveStudio\Clients\\LabClient.dll'
[14:39:51] GM: 1 Guest (s) init
[14:39:51] GM: 1 Module(s) init
[14:39:51] GM: 2 Tab (s) init
[14:39:51] RSTD.Client_LoadXml()
[14:39:51] [RadarAPI]: ar1.selectRadarMode(0)
[14:39:51] [RadarAPI]: Status: Passed
[14:39:51] Matlab Runtime Engine is installed
[14:39:51] [RadarAPI]: Starting Matlab Engine..
[14:39:56] [RadarAPI]: Matlab Engine Started!
[14:39:58] [RadarAPI]: ar1.selectCascadeMode(0)
[14:39:58] [RadarAPI]: Status: Passed
[14:39:58] [RadarAPI]: ar1.LoadSettings('C:\Users\x0108845\AppData\Roaming\RSTD\ar1gui.ini')
[14:39:59] TESTING = false
[14:39:59] RstdNet: Port 2777: Listening..
[14:39:59] [RadarAPI]: ar1.SelectCaptureDevice("DCA1000")
[14:39:59] [RadarAPI]: Status: Passed
[14:40:00] [RadarAPI]: Opening Gpio Control Port()
[14:40:00] [RadarAPI]: Status: Passed
[14:40:00] [RadarAPI]: Opening Board Control Port()
[14:40:00] [RadarAPI]: Status: Passed
[14:40:01] [RadarAPI]: ar1.FullReset()
[14:40:01] [RadarAPI]: Status: Passed
[14:40:02] [RadarAPI]: Closing Board Control Port()
[14:40:02] [RadarAPI]: Status: Passed
[14:40:02] [RadarAPI]: Closing Gpio Control Port()
[14:40:02] [RadarAPI]: Status: Passed
[14:40:02] [RadarAPI]: ar1.SOPControl(2)
[14:40:02] [RadarAPI]: Status: Passed
[14:40:03] [RadarAPI]: ar1.Connect(12,921600,1000)
[14:40:06] [RadarAPI]: Warning: Connected with baudrate 115200
[14:40:07] [RadarAPI]: Warning: Disconnected existing BaudRate
[14:40:07] [RadarAPI]: Warning: Trying to connect with baudrate 921600
[14:40:09] [RadarAPI]: ar1.Calling_IsConnected()
[14:40:10] [RadarAPI]: ar1.SelectChipVersion("AR1642")
[14:40:10] [RadarAPI]: Status: Passed
[14:40:10] [RadarAPI]: ar1.SelectChipVersion("AR1642")
[14:40:10] [RadarAPI]: Status: Passed
[14:40:10] [RadarAPI]: ar1.deviceVariantSelection("XWR1642")
[14:40:10] [RadarAPI]: Status: Passed
[14:40:10] [RadarAPI]: ar1.frequencyBandSelection("77G")
[14:40:10] [RadarAPI]: ar1.SelectChipVersion("XWR1642")
[14:40:10] [RadarAPI]: Status: Passed
[14:40:10] Device Status : XWR1642/ASIL-B/SOP:2/ES:2
[14:40:11] [RadarAPI]: ar1.DownloadBSSFw("C:\\ti\\mmwave_studio_02_01_01_00\\rf_eval_firmware\\radarss\\xwr12xx_xwr14xx_radarss.bin")
[14:40:12] [RadarAPI]: Downloading BSS Patch RPRC Binary..
[14:40:13] [RadarAPI]: ar1.GetBSSFwVersion()
[14:40:13] [RadarAPI]: BSSFwVersion:(02.00.00.01 (05/10/17))
[14:40:14] [RadarAPI]: ar1.GetBSSPatchFwVersion()
[14:40:14] [RadarAPI]: BSSPatchFwVersion:(01.02.05.02 (30/04/19))
[14:40:16] [RadarAPI]: ar1.DownloadMSSFw("C:\\ti\\mmwave_studio_02_01_01_00\\rf_eval_firmware\\masterss\\xwr12xx_xwr14xx_masterss.bin")
[14:40:17] [RadarAPI]: Downloading MSS RPRC Binary..
[14:40:20] [RadarAPI]: ar1.GetMSSFwVersion()
[14:40:20] [RadarAPI]: MSSFwVersion:(01.02.05.01 (12/07/19))
[14:40:22] [RadarAPI]: ar1.PowerOn(0, 1000, 0, 0)
[14:40:22] [RadarAPI]: Status: Passed
[14:40:22] MSS power up done async event received!
[14:40:23] [RadarAPI]: ar1.SelectChipVersion("AR1642")
[14:40:23] [RadarAPI]: Status: Passed
[14:40:23] [RadarAPI]: ar1.SelectChipVersion("XWR1642")
[14:40:23] [RadarAPI]: Status: Passed
[14:40:24] Device Status : XWR1642/ASIL-B/SOP:2/ES:2
[14:40:24] [RadarAPI]: ar1.RfEnable()
[14:40:24] BSS power up done async event received!
[14:40:24] [RadarAPI]: Status: Passed
[14:40:24] [RadarAPI]: ar1.GetMSSFwVersion()
[14:40:24] [RadarAPI]: MSSFwVersion:(01.02.05.01 (12/07/19))
[14:40:24] [RadarAPI]: ar1.GetBSSFwVersion()
[14:40:25] [RadarAPI]: BSSFwVersion:(02.00.00.01 (05/10/17))
[14:40:25] [RadarAPI]: ar1.GetBSSPatchFwVersion()
[14:40:25] [RadarAPI]: BSSPatchFwVersion:(01.02.05.02 (30/04/19))
[14:40:25] [RadarAPI]: ar1.ChanNAdcConfig(1, 1, 0, 1, 1, 1, 1, 2, 1, 0)
[14:40:26] [RadarAPI]: Status: Passed
[14:40:26] [RadarAPI]: ar1.LPModConfig(0, 0)
[14:40:26] [RadarAPI]: Status: Failed, Error Type: REGULAR ADC MODE NOT SUPPORTED IN 5 MHz PART VARIANT DEVICE
[14:40:26] [RadarAPI]: ar1.RfInit()
[14:40:26] RF Init async event received!
[14:40:26] [RadarAPI]: Time stamp, Temperture: 2163,40; APLL Status, Update: 1, 0; SynthVCO1 Status, Update: 1, 1; SynthVCO2 Status, Update: 1, 1; LODist Status, Update: 1, 1; RxADCDC Status, Update: 1, 1; HPFcutoff Status, Update: 1, 1; LPFcutoff Status, Update: 1, 1; PeakDetector Status, Update: 1, 1; TxPower Status, Update: 1, 1; RxGain Status, Update: 1, 1; TxPhase Status, Update: 0, 0; RxIQMM Status, Update: 1, 1;
[14:40:26] [RadarAPI]: Status: Passed
[14:40:27] [RadarAPI]: ar1.DataPathConfig(1, 1, 0)
[14:40:27] [RadarAPI]: Status: Passed
[14:40:27] [RadarAPI]: ar1.LvdsClkConfig(1, 1)
[14:40:27] [RadarAPI]: Status: Passed
[14:40:27] [RadarAPI]: ar1.LVDSLaneConfig(0, 1, 1, 1, 1, 1, 0, 0)
[14:40:27] [RadarAPI]: Status: Passed
[14:40:27] [RadarAPI]: ar1.SetTestSource(4, 3, 0, 0, 0, 0, -327, 0, -327, 327, 327, 327, -2.5, 327, 327, 0, 0, 0, 0, -327, 0, -327, 327, 327, 327, -95, 0, 0, 0.5, 0, 1, 0, 1.5, 0, 0, 0, 0, 0, 0, 0)
[14:40:27] [RadarAPI]: Status: Passed
请尝试把采样率设置在6.25Mbps以内。请看数据手册对采样率的要求。
6 Device Comparison
https://www.ti.com/lit/ds/symlink/awr1642.pdf