Part Number: AWR1443BOOST
你好,请问mmWave Studio这个“No of Chirp Loops”(如下图)是指的是每一帧内,每个发射天线发出的Chirp波各是128个,还是几根发射天线发出的总chirp数是128呢?

This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: AWR1443BOOST
你好,请问mmWave Studio这个“No of Chirp Loops”(如下图)是指的是每一帧内,每个发射天线发出的Chirp波各是128个,还是几根发射天线发出的总chirp数是128呢?

一帧内的chirp总数是"Start Chirp Tx" 到 "End Chirp Tx" 循环 "no of chirp loops" ,是每根天线各128。
相邻两个chirp是来自不同的发射天线的吗
是的。
存储格式请参考以下文档 xWR12xx and xWR14xx With DCA1000 Data Format:
如果这么说的话,那我使用2根发射天线,4根接收天线,采集250帧数据,No of Chirp Loops设为128,每帧采样数为256的话,那应该得到256(采样数)x128(No of Chirp Loops)X2(发射天线)x4(接收天线)x250(帧数)=65536000个数据,但我16进制转10进制后,只有一般的数据量,请问确实是每根发射天线各发128个chirp吗?
公式如下:
Total Size in Bytes = Num ADC Samples × Num RX Channels × Num Frames × Num Chirps × Num Bytes Per Sample
For a complex output format, there are 4 bytes per sample: 2 bytes for the real part and 2 bytes for the imaginary part. For a real output format, there are 2 bytes per sample.
"Start Chirp Tx" 到 "End Chirp Tx" 循环 "no of chirp loops"
一帧时间内两根发射天线发出的Chirp总数是128吗
(End chirp index - start chirp index+ 1) * number of chirp loops.
我之前描述有误, Chirp Start Index表示第一个chirp号,Chirp End Index表示最后一个chirp号,这些chirp有同样的参数如 ProfileId、StartFreqVar、FreqSlopeVar、IdleTimeVar、ADCStartVar 和 TXEnable等。
参考以下帖子中的解释: