Part Number: AWR1642
Other Parts Discussed in Thread: SYSBIOS
您好,我在SRR demo的基础上进行代码修改,我只启用了USRR模式
在mss_srr_cli.c文件中,我添加了新的CLI命令及其回调函数
cliCfg.tableEntry[4].cmd = "reconfiguration";
cliCfg.tableEntry[4].helpString = "Idle time";
cliCfg.tableEntry[4].cmdHandlerFxn = SRR_MSS_CLIChirpReconfiguration;
static int32_t SRR_MSS_CLIChirpReconfiguration(int32_t argc, char* argv[])
{
int32_t retVal;
rlDynChirpCfg_t dynChirpCfg[1U];
unsigned int cnt;
dynChirpCfg[0].chirpRowSelect=0x30; //Enables only chirp row 3 to be reconfigured
dynChirpCfg[0].chirpSegSel=0;
dynChirpCfg[0].programMode=0;
for(cnt=0;cnt<2;cnt++)
{
dynChirpCfg[0].chirpRow[cnt].chirpNR3=(rlUInt32_t)atoi(argv[0]);
}
rlDynChirpCfg_t *dynChirpData[1]=&dynChirpCfg[0];
retVal=rlSetDynChirpCfg(RL_DEVICE_MAP_INTERNAL_BSS,4U,&dynChirpData[0]);
/* Check for mmWaveLink API call status */
if (retVal != RL_RET_CODE_OK)
{
System_printf("Error: Unable to configure the dynamic chirp [Error %d]\n",retVal);
return -1;
}
rlDynChirpEnCfg_t dynChirpEnCfg = {0};
retVal = rlSetDynChirpEn(RL_DEVICE_MAP_INTERNAL_BSS, &dynChirpEnCfg);
if(retVal != RL_RET_CODE_OK)
{
/* Error: Link reported an issue. */
System_printf("Error: rlSetDynChirpEn retVal=%d\n", retVal);
return -1;
}
return 0;
}
在调试时,CLI命令advFrameCfg和sensorStart执行得很好,但输入自定义的reconfiguration命令后出现以下错误:
[Cortex_R4_0] Debug: Launched the Initialization Task
Debug: Initialized the mmWave module
Debug: Synchronized the mmWave module
Debug: CLI is operational
[C674X_0] Heap L1 : size 16384 (0x4000), free 1216 (0x4c0)
Heap L3 : size 786432 (0xc0000), free 229376 (0x38000)
Heap L2 : size 49152 (0xc000), free 27040 (0x69a0)
[Cortex_R4_0] Debug: MMWave has been configured for SRR.
Debug: Sensor will start momentarily.
Exception occurred in ThreadType_Task.
Task handle: 0x8005ce0.
Task stack base: 0x8005d40.
Task stack size: 0x1000.
R0 = 0x00000000 R8 = 0xffffffff
R1 = 0x00000000 R9 = 0x080099a0
R2 = 0x08006a28 R10 = 0x0800985c
R3 = 0x00000001 R11 = 0xffffffff
R4 = 0x00000000 R12 = 0x00000000
R5 = 0x00000000 SP(R13) = 0x08006b60
R6 = 0x00010000 LR(R14) = 0x00009919
R7 = 0x00000007 PC(R15) = 0x00080000
PSR = 0x400c019f
DFSR = 0x00000000 IFSR = 0x0000000d
DFAR = 0x00000000 IFAR = 0x00080000
ti.sysbios.family.arm.exc.Exception: line 201: E_prefetchAbort: pc = 0x00080000, lr = 0x00009919.
xdc.runtime.Error.raise: terminating execution
请问这个问题该如何解决?