Part Number: IWR1443
Hello friends, I have encountered a tricky problem.
I am sending .cfg configuration files to an IWR1443 development board through MATLAB, which allows the radar to collect data. However, after successfully sending the .cfg file once and the board working correctly, MATLAB is unable to send the .cfg file to the board, or the process of sending the .cfg file is very slow (taking more than 20 minutes).
The first time the .cfg file was sent to the board, everything worked normally

After that, MATLAB's program is unable to send .cfg files to the development board normally。As shown in the figure below, it seems that MATLAB did not send the configuration file to XWR1xxx 11.cfg properly.

I sincerely hope that my friends can provide valuable suggestions!Thanks!