Part Number: AWR1843BOOST
如题,pa例程中的mss和dss分别是什么意思?
bss部分内容及设置在哪里可以看到?
pa例程只有mss工程和dss。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
看的是C:\ti\mmwave_sdk_03_05_00_04\packages\scripts\ImageCreator\Image_Creator_User_Guide.pdf文档里面的三个.out文件。下图是截图,我看pa项目,打开ccs只有mss和dss,那么bss有用到吗?它是融合进mss和dss工程了?

sdk中会提供对应的固件,是控制mmwave射频前端的,更详细的介绍可查看以下培训视频。
Introduction to mmWave SDK
www.ti.com/.../mmwave-training-series.html
mmwave_sdk_03_05_00_04-Windows-x86-Install\mmwave_sdk_03_05_00_04\firmware\radarss
The Radar SS Firmware or the mmWave Front End controls the RF and the analog hardware blocks and is responsible for the entire mmWave Radar operations. The mmWaveLink is the driver for the Radar SS Firmware and provides low level APIs to control each of the hardware blocks in the front end.
你好,请问,我在TI Resource Explorer中搜索文档ERRATA,如下图1所示,其中4.1小节,MSS的三线模式是什么意思?谢谢。另外,ERRATA文档中第5节,如图2,这些是mss中的错误或者警告类型吗?我没有看到dss相关的错误内容说明。请问dss的在哪里?