This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

IWR1843BOOST: [C674X_0] {module#8}: "../dss_main.c", line 252: error {id:0x10000, args:[0x816904, 0x816904]} xdc.runtime.Error.raise: terminating execution

Part Number: IWR1843BOOST
Other Parts Discussed in Thread: AWR1843, IWR1843

工程师你好,

我将AWR1843的pa_18xx_dss、pa_18xx_dss代码运行在IWR1843平台,发现ADCBUF有数据在更新。

但是DSP出现这样的错误,

[C674X_0] {module#8}: "../dss_main.c", line 252: error {id:0x10000, args:[0x816904, 0x816904]}
xdc.runtime.Error.raise: terminating execution

错误代码:

        if (gMrrDSSMCB.frameStartIntToken == 1)
        {
            gMrrDSSMCB.frameStartIntToken = 0;

            dataPathObj = &gMrrDSSMCB.dataPathObj[0];

            /* Increment event stats */
            gMrrDSSMCB.stats.frameStartEvt++;

            /* Check if the previous frame has been completely processed. */
            MmwDemo_dssAssert(dataPathObj->chirpCount != 0);
        }

请问这是什么原因

  • 请问是如何调试的?两个core全速跑的情况下吗?

  • 首先运行的DSS,然后运行的MSS,之后在串口助手输入命令advFrameCfg sensorStart,

    我不懂什么是全速调试

  • 我觉得您应该说的是这个

  • 两个core全速跑的情况下吗

    4. Execute the Lab

    mmwave_automotive_toolbox_3_4_0\labs\lab0008_automated_parking\docs\APdemo_usersguide.pdf

    按照user guide中测试有问题吗?

  • 我按照group执行了一遍,然后串口输入以下命令,但是没有串口返回数据

    ******************************************
    xWR18xx MMW Demo 03.05.00.04
    ******************************************
    mmwDemo:/>PaTIDesign:/>advFrameCfg
    Done
    PaTIDesign:/>
    PaTIDesign:/>sensorStart
    Done
    PaTIDesign:/>
    PaTIDesign:/>

  • 现象就是程序一直在以下两个函数内交替运行

    static void MRR_DSS_frameStartIntCallback(uintptr_t arg)
    {
        gMrrDSSMCB.frameStartIntToken = 1;
        gMrrDSSMCB.stats.frameStartIntCounter++;
        return;
    }
    static void MRR_DSS_chirpIntCallback(uintptr_t arg)
    {
        gMrrDSSMCB.chirpProcToken = 1;
        gMrrDSSMCB.stats.chirpIntCounter++;
        return;
    }

    但是不能进入数据处理的任务MmwDemo_interFrameProcessing和MmwDemo_processChirp

  • 我按照group执行了一遍,然后串口输入以下命令,但是没有串口返回数据

    ******************************************
    xWR18xx MMW Demo 03.05.00.04
    ******************************************
    mmwDemo:/>PaTIDesign:/>advFrameCfg
    Done
    PaTIDesign:/>
    PaTIDesign:/>sensorStart
    Done
    PaTIDesign:/>
    PaTIDesign:/>

    这边是如何进行测试的,我在GUI中测试的是成功的。

  • 这边是如何进行测试的,我在GUI中测试的是成功的。

    1.连接两个core

    2依此加载DSS、MSS的程序.

    3.点击group ,点击Resume

    4.console打印调试信息,针对out of DDR heap 问题,我将#define SUBFRAME_USRR_LOOP_COUNT   从64改成4,不知道什么原因

    [Cortex_R4_0] Debug: Launched the Initialization Task
    [C674X_0] out of DDR heap memory!
    processCreate: (radarProcessInstance_t *)0x806a78
    [Cortex_R4_0] Debug: Initialized the mmWave module
    [C674X_0] processCreate: (RADARDEMO_rangeProc_handle *)0xc00ccaf8
    [Cortex_R4_0] Debug: Synchronized the mmWave module
    [C674X_0] processCreate: (RADARDEMO_dopplerProc_handle *)0x806b78
    [Cortex_R4_0] Debug: CLI is operational
    [C674X_0] processCreate: (RADARDEMO_detectionCFAR_handle *)0x806e60
    processCreate: (RADARDEMO_aoAEstBF_handle *)0x807e5c
    processCreate: (RADARDEMO_clusteringDBscanInstance *)0x80df00
    processCreate: (radarProcessBenchmarkObj *)0x80ff8c
    processCreate: heatmap (float *)0x0
    radar process create error! Exit!DDR Heap : size 786432 (0xc0000), used 851968 (0xd0000)
    LL2 Heap : size 61440 (0xf000), used 58312 (0xe3c8)
    LL2 Scratch : size 8192 (0x2000), used 6656 (0x1a00)
    LL1 Scratch : size 16384 (0x4000), used 16384 (0x4000)
    HSRAM Heap : size 0 (0x0), used 0 (0x0)

    5.开启串口助手,COM3(命令串口),COM4(数据串口)

    6.可以看到console控制台有返回信息

    Debug: MMWave has been configured for MRR.
    Debug: Sensor will start momentarily.

    7.COM4(数据串口)没返回数据信息

  • GUI窗口发出命令是这样的,但是貌似也没有数据返回

  • 当#define SUBFRAME_USRR_LOOP_COUNT                (16U)会出现错误

     xdc.runtime.Main: "../mss_main.c", line 194: assertion failure
    xdc.runtime.Error.raise: terminating execution

    能否将您运行在IWR1843的代码发一下

  • 数据口Tx上能测到数据输出吗?返回done应该是成功了。

    我不太清楚您说的数据返回是有参考过哪个文档吗?

    GUI运行之后是正常能跑起来吧?

  • .屏蔽了MSS里的监听器配置,程序就会有数据输出,但是如果没有屏蔽会出现以下错误

    //    /* Register Chirp Available Listener */
    //    memset ((void*)&listenerCfg, 0, sizeof(SOC_SysIntListenerCfg));
    //    listenerCfg.systemInterrupt   = SOC_XWR18XX_MSS_CHIRP_AVAIL_IRQ;
    //    listenerCfg.listenerFxn       = MRR_MSS_chirpIntCallback;
    //    listenerCfg.arg               = 0;
    //    gMrrMSSMCB.chirpIntHandle = SOC_registerSysIntListener (gMrrMSSMCB.socHandle, &listenerCfg, &errCode);
    //    if (gMrrMSSMCB.chirpIntHandle == NULL)
    //    {
    //        System_printf ("Error: Unable to register the Chirp Available Listener [Error code %d]\n", errCode);
    //        return;
    //    }
    //
    //    /* Register Frame Start Listener */
    //    memset ((void*)&listenerCfg, 0, sizeof(SOC_SysIntListenerCfg));
    //    listenerCfg.systemInterrupt   = SOC_XWR18XX_MSS_FRAME_START_INT;
    //    listenerCfg.listenerFxn       = MRR_MSS_frameStartIntCallback;
    //    listenerCfg.arg               = 0;
    //    gMrrMSSMCB.frameStartIntHandle = SOC_registerSysIntListener (gMrrMSSMCB.socHandle, &listenerCfg, &errCode);
    //
    //    if (gMrrMSSMCB.frameStartIntHandle == NULL)
    //    {
    //        System_printf("Error: Unable to register the Frame start Listener [Error code %d]\n", errCode);
    //        return ;
    //    }

    xdc.runtime.Main: "../mss_main.c", line 194: assertion failure
    xdc.runtime.Error.raise: terminating execution

    错误来源:

  • 好的,感谢分享!