This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

FDC2112: 采集数据不正确

Part Number: FDC2112

如下图所示是我的应用系统,FDC2112配置是

CH0_FIN_SEL为b10

CH0_FREF_DIVIDER 为0x01

DRIVE_CURRENT_CH0为0xA800,示波器测试INA0的波形Vpp为1.5V

SETTLECOUNT register (0x10) is 0x000E.

CH0_RCOUNT register (0x08) to 0x186A

CONFIG register (address 0x1A) is 0x1681,单端配置,OUTPUT_GAIN为1,外部时钟源

这样的配置,从DATA_CH0寄存器读出的值为0x33C,按照手册公式计算出来的等效电容为348pf,但我的SMA接头未接任何东西,C1和C2各33pf,应为66pf,即使PCB板上线有寄生电容,也不至于有接近300pf的大小。

另外,我在SMA上SIGNAL和GND之间外接50pf电容时,DATA_CH0寄存器读出的值为0x338,变化量很小,折算出来只有几pf的变化量,这与实际不一致。