This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AWR2944: AWR2944芯片在DDMA模式是否支持advance frame配置

Part Number: AWR2944


您好,我在使用AWR2944芯片时,在DDMA模式想利用双波形交替发射进行速度扩展,在查看相关TI文档后看到有advanceframe模式能够实现该发射模式,在配置完成后发现代码运行到MmwDemo_configPhaseShifterChirps函数模块中会判断如果dfeDataOutputMode为MMWave_DFEDataOutputMode_ADVANCED_FRAME,则运行到CLI_write("Advanced Subframe Config is not currently supported with the DDMA chain\n")。因此想请问下AWR2944芯片实际是否支持在DDMA模式下使用advance frame配置,如果可以,那么我该在哪些地方来修改来实现该功能?谢谢!