Other Parts Discussed in Thread: LDC1101, LDC1612
“在探头谐振检测电路的采样过程中,LDC 1614电感数字转换芯片中存在一个高频振荡器,不断输出扫频信号。当检测探头的LC网络谐振时,LC谐振电路的阻抗最大,检测电路的输出电压最大。通过保持输出信号的频率,最大输出电压保持恒定,从而可以将LC电路保持在谐振状态。”
以上表述是否正确,LDC1614内部是有高频振荡器吗,LDC1101是不是同样的原理
谢谢
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好,
您是在问 LDC1614的工作原理吗?如 datasheet 7.2 Functional Block Diagram部分所述,LDC1612/LDC1614 前端是谐振电路驱动器,然后是多路复用器,将各通道连接到测量和数字化传感器频率(ƒsensor)的核。核使用参考频率(ƒREF)来测量传感器频率。ƒREF源自内部参考时钟(振荡器)或外部提供的时钟。每个通道的数字化输出与ƒSENSOR/ƒREF的比率成比例。I2C接口用于支持设备配置并将数字化的频率值传输到主处理器。

LDC1101测量电感的工作原理是一样的,但是LDC1101还可以测LC振荡器的阻抗,如下LDC1101 datasheet 8.1的Overview描述:

LDC1101是一种电感数字转换器,可以同时测量LC谐振器的阻抗和谐振频率。高分辨率测量能力使该设备能够用于直接测量物理系统的变化,从而使谐振器能够感测导电材料的接近和移动。
LDC1101通过将闭环配置中的振荡幅度调节在恒定水平来测量阻抗和谐振频率,同时监测谐振器耗散的能量。通过监测注入谐振器的功率量,LDC1101可以确定谐振器的等效并联电阻RP,并将其作为数字值返回。
此外,LDC1101装置还通过将传感器频率与所提供的参考频率进行比较来测量LC电路的振荡频率。然后可以使用传感器频率来确定LC电路的电感。
阈值比较器块可以将RP+L转换结果与可编程阈值进行比较。通过编程阈值寄存器并启用比较器,LDC1101可以提供开关输出,报告为INTB/SDO引脚上的高/低电平。
LDC1101设备支持范围广泛的LC组合,振荡频率范围从500 kHz到10 MHz,RP范围从1.25 kΩ到90 kΩ。该设备通过简单的4线SPI进行配置并检索转换结果。
最后下面FAQ希望对您有帮助: