由于中秋、国庆节假期,帖子审批以及工程师回复将会有所延迟,敬请谅解.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AWR6843ISK: 当配合DCA1000采集数据时,能否同时在AWR6843上运行嵌入式应用?

Part Number: AWR6843ISK
Other Parts Discussed in Thread: DCA1000EVM

当AWR6843ISK和DCA1000搭配使用时,我希望能同时实现两种目的:

  1. 毫米波数据直接利用AWR6843ISK的计算资源进行处理并展示(例如运行TI提供的Occupancy & Vital Signs Detection Lab,或者我们自己通过CCS IDE开发的程序);
  2. 毫米波数据通过DCA1000传输并储存在电脑上(DCA1000的基本功能)。

我的问题在于,以上两点能否利用一套6843+DCA1000设备同时实现?希望能提供相关资料,感谢!

  • 毫米波数据直接利用AWR6843ISK的计算资源进行处理并展示(例如运行TI提供的Occupancy & Vital Signs Detection Lab,或者我们自己通过CCS IDE开发的程序);

    这个不需要DCA1000EVM板,单独用ISK板子就可以了。

    以上两点能否利用一套6843+DCA1000设备同时实现?

    不是很明白您的需求,是不想用mmwave studio,然后在Occupancy & Vital Signs Detection Lab里实现DCA1000EVM原始数据的采集?

  • Occupancy & Vital Signs Detection Lab里实现DCA1000EVM原始数据的采集

    是的,我的疑问在于,DCA1000的数据采集与6843的MCU计算是否形成冲突?如果不冲突,那么是否存在某种软硬件设置,允许只利用一组设备同时实现毫米波原始数据采集AWR6843ISK雷达嵌入式计算

  • 那么是否存在某种软硬件设置,

    DCA1000 mode和function mode拨位键配置不同。