This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

PGA302: PGA302

Part Number: PGA302
Other Parts Discussed in Thread: PGA305

Dear supporter:

         Q1: PGA302是否可以通过I²C输出数字格式的传感器数据?

        Q2:PGA302与PGA305相比,精度范围如何?

  • Q1: PGA302是否可以通过I²C输出数字格式的传感器数据?

    I 2C 接口是用来配置其他功能的,可以看下register maps。 不是ADC的数字输出。

    Q2:PGA302与PGA305相比,精度范围如何?

    两款都是高精度传感器,并且功能相似,但是也有差异,在 PGA305,您可以使用 I2C 运行时命令通过 I2C 读取补偿后的24位数据。 在 PGA302上,您只能读取原始 ADC 数据。 

    另外,PGA302 和PGA305的output rate也是不同的。所以可以根据自己的实际应用去决定选择哪款sensor。