This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

HDC2010: 温湿度传感器湿度误差是什么问题

Part Number: HDC2010

测试目的:测试HDC2010的温湿度精确度

测试设备:可程式恒温恒湿箱

测试样机数量:8台样品和1台对比机

测试条件:温度15℃,湿度60%,用时5个小时

测试方法:将8台设备和1台对比机放置可程式恒温恒湿箱内,设置温度为15℃,湿度60%,开始启动设备,等待3小时后开始读取设备,的温湿度值隔一个小时后再次读取设备的温湿度值,一共读取3次,数值发现有两台湿度偏大如图片所示

发现5号和8号湿度达到66%RH,这两个机型的湿度偏大,温度所有机型都没有问题,请问这种误差是否正常,是什么原因造成的,这种5 号和8号产品该如何处理?

  • 您好,

    建议您先确认焊接时是否遵循下面链接文档中的Table 2 and Figure 3 曲线进行焊接的?

     https://www.ti.com/lit/an/spraby1a/spraby1a.pdf 

    您可以在这两个板上运行加热器(发送0x08到寄存器0x0E) 5-10分钟左右,然后查看%RH误差是否降低回或接近正常/预期水平。 (当然是在零件冷却后) 

     if they could operate the heater (send 0x08 to register 0x0E) on a few boards for 5-10min or so, and then see if the %RH error decreases back to or close to normal/expected levels. (after the part cools down, of course)

    下面文档列出了要检查的其他事项,包括已知会影响传感器元件的化学品等:

    https://www.ti.com/lit/ug/snau250/snau250.pdf