This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AWR1642: 配置高级帧subframe报错

Part Number: AWR1642

首先是profile和chirp的配置

配置完之后,转到advframeconfig页面,按照下图进行配置

配置完之后点击set,之后点击下图中的set

之后会提示上图中的错误,Status: Failed, Error Type: FRAME ARE ALREADY STOPPED WHEN THE FRAME_STOP COMMAND WAS ISSUED

翻译一下为:状态:失败,错误类型:当发出帧停止命令时帧已经停止

我还没有点击开始采集。还麻烦各位大神指点一二。