This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AWR2944: AWR2944的SDK4.4.1中HWA的Zeroinsert功能配置问题

Part Number: AWR2944

你好,工程师

我想把原来运行在SDK4.3.1版本中的代码移植到SDK4.4.1版本,移植相同的代码到SDK4.4.1,发现编译出来的appimage文件不能正常运行,经过排查发现是HWA中的ZeroInsert部分的配置导致的;

因为SDK4.4.1使用的是HWA2.1,SDK4.3.1使用的是HWA2.0,两者在ZeroInsert部分的配置存在不同,见TRM文档

之前在HWA2.0中配置如下:

在函数DPU_DopplerProcHWA_configHwaCFARAzimFFT中

hwaParamCfg[paramsetIdx].accelModeArgs.fftMode.preProcCfg.zeroInsertEn=HWA_FEATURE_BIT_ENABLE;

在DPU_DopplerProcHWA_config中

obj->dopplerAzimHwaCommonConfig.configMask |=HWA_COMMONFIG_MASK_ZEROINSERT_NUM_MASK;

obj->dopplerAzimHwaCommonConfig.zeroInsertConfig.number=6;

obj->dopplerAzimHwaCommonConfig.zeroInsertConfig.mask[0]=0x2BDEF5;

请问在HWA2.1中应该如何配置ZeroInsert功能?

谢谢