Dears,
Would you please help to advise the difference between LM19CIZ/LFT4 and LM19CIZ/NOPB?
Are they PTP? Thanks.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Dears,
Would you please help to advise the difference between LM19CIZ/LFT4 and LM19CIZ/NOPB?
Are they PTP? Thanks.
Hello,
the LFT4 is tape and reel and comes in package quantity of 2kU, NOPB is bulk pack with package quantity of 1800.
Please see this application note regarding all the suffixes possible for the TO-92 parts
https://www.ti.com/lit/an/snoa072a/snoa072a.pdf
Are they PTP?
Yes, they have the same package type and same electrical characteristics, the differences are only the pack and quantity.
Just found that there is pin pitch difference.
Sorry for your reply you so late due to Vacation Leave last week.
Do you mean that LM19CIZ/LFT4 and LM19CIZ/NOPB have the pitch difference?
Seems yes. Would you please help to confirm? Thanks.
Hi, do you have the pictures? Please attach the pictures which is convenience to confirm.
In addition, if you bought them by distributor, please also attach the order number.
Hello, I have confirmed that:
The difference between NOPB and LFT4 is the packing options:
Please see the following application notes for more information on the packing suffixes.
https://www.ti.com/lit/an/snoa072a/snoa072a.pdf