如果我将CFAR_OUT_MODE此参数寄存器设置为10或11(检测峰值列表模式),他只会输出检测到的峰值目标的信息,但在运行前我并不清楚有几个峰值目标,那么我的输出格式化器中的DSTANCT、DSTAINDX、DSTBINDX应该如何设置。
并且我发现在介绍中存在一个FFTPEAKCNT寄存器,此寄存器会表示有多少个峰值目标,以便于主处理器来拿多少个样本,那么我想问的是,此寄存器是会统计当前运行的参数集的多次迭代的总和峰值目标吗,还是一次迭代的峰值目标(迭代:REG_BCNT)。如果是一次迭代的峰值目标个数,那此时当前参数集并未运行完成,第二次迭代的峰值目标个数不会将第一次迭代的峰值目标个数给覆盖吗?如果是多次迭代的峰值目标,那么在不清楚峰值目标个数的情况下(设置参数寄存器)我如果使用输出格式化器将这多次迭代的峰值样本个数给连续存储到目标内存(MEM_2,3)?
输出模式选择的是峰值列表模式输出,此时的DSTBINDX为什么设置的是0值,这样对于多次迭代下的输出数据不会反复覆盖吗