This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AWR2243: 如何使用DEV_TESTPATTERN_GEN_SET_SB发送模拟数据

Part Number: AWR2243


你好,

       我这边按照官网给的demo程序mmWareLink_SingleChip_Example做移植,已可以通过CSI接口上传ADC数据;目前想验证FPGA解析数据的正确性,希望使用DEV_TESTPATTERN_GEN_SET_SB对4路Rx做一组递增的测试数据,触发CSI接口上传到FPGA,但是CSI接口上并没有任何数据发出,请问这个功能应该如何使用?

       我这边是基于mmWareLink_SingleChip_Example的程序,在配置Frame参数和使能Frame Start之前,增加了DEV_TESTPATTERN_GEN_SET_SB的设置,其余配置还是和demo完全一样(请问是否要关掉部分配置?)

配置参数如下图,chirp设置为128个,采样点是256,只有实部数据