This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DCA1000EVM: 无法加载 DLL“mclmcrrt8_5_1.dll”: 找不到指定的模块。 (异常来自 HRESULT:0x8007007E)。

Part Number: DCA1000EVM


[17:09:40] RSTD.SetVar ("/Settings/Clients/Client 0/GuiDll" , "")
[17:09:40] RSTD.SetVar ("/Settings/AutoUpdate/Enabled" , "TRUE")
[17:09:40] RSTD.SetVar ("/Settings/AutoUpdate/Interval" , "1")
[17:09:40] RSTD.SetVar ("/Settings/Monitors/UpdateDisplay" , "TRUE")
[17:09:40] RSTD.SetVar ("/Settings/Monitors/OneClickStart" , "TRUE")
[17:09:40] RSTD.SetVar ("/Settings/Automation/Automation Mode" , "false")
[17:09:40] RSTD.Transmit("/")
[17:09:40] RSTD.SaveSettings(): Settings saved to "C:\Users\LENOVO\AppData\Roaming\RSTD\config.xml"
[17:09:40] RSTD.Build()
[17:09:40] RSTD.SaveSettings(): Settings saved to "C:\Users\LENOVO\AppData\Roaming\RSTD\config.xml"
[17:09:40] RSTD.Transmit("/")
[17:09:40] RSTD.AL_Build()
[17:09:40] RSTD.AL_LoadXml()
[17:09:40] RSTD.Transmit("/")
[17:09:40] RSTD.AL_Init()
[17:09:40] RSTD.Clients_Build()
[17:09:40] GM: Init
[17:09:40] GM: Loaded 'C:\ti\mmwave_studio_02_01_01_00\mmWaveStudio\Clients\\LabClient.dll'
[17:09:40] GM: 1 Guest (s) init
[17:09:40] GM: 1 Module(s) init
[17:09:40] GM: 2 Tab (s) init
[17:09:40] RSTD.Client_LoadXml()
[17:09:41] [RadarAPI]: ar1.selectRadarMode(0)
[17:09:41] [RadarAPI]: Status: Passed
[17:09:41] Matlab Runtime Engine is installed
[17:09:41] [RadarAPI]: Starting Matlab Engine..
[17:09:41] [RadarAPI]: Error: “MatlabPostProcGui.MatlabPostProcGUIClass”的类型初始值设定项引发异常。
[17:09:41] Trace:
[17:09:41] 在 MatlabPostProcGui.MatlabPostProcGUIClass..ctor()
[17:09:41] 在 AR1xController.frmAR1Main.InitMatlabPostProcEngine(String PostProcesspath)
[17:09:41] [RadarAPI]: Error: Error occured in Matlab Initialization
[17:09:41] [RadarAPI]: Matlab Engine couldn't be Started..
[17:09:42] [RadarAPI]: ar1.selectCascadeMode(0)
[17:09:42] [RadarAPI]: Status: Passed
[17:09:42] [RadarAPI]: ar1.LoadSettings('C:\Users\LENOVO\AppData\Roaming\RSTD\ar1gui.ini')
[17:09:42] [RadarAPI]: Error: 未将对象引用设置到对象的实例。
[17:09:42] Trace:
[17:09:42] 在 AR1xController.ScriptOps.getMatlabPostProcVersion()
[17:09:42]
[17:09:42] &&&&&&&&&&&&&&&&&&&&
[17:09:42] ***Script FAILED!***
[17:09:42] &&&&&&&&&&&&&&&&&&&&
[17:09:42] Exception message is:
[17:09:42] 无法加载 DLL“mclmcrrt8_5_1.dll”: 找不到指定的模块。 (异常来自 HRESULT:0x8007007E)。

我已经安装了手册对应的东西,但是还是会报这个错误,用的是win11,请问是什么问题