This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AWR2243: 硬触发连续采样问题

Part Number: AWR2243


您好,我这边在使用AWR2243的级联模式,想做连续采样,采样的方式是触发一帧,收到数据后我再控制触发下一帧。目前1个2243作为mater,11个2243作为slave,其中master的触发配置为软件模式、slave的触发配置为硬件模式,需要咨询的问题如下:

1.  第一次触发采样,是否所有的awr2243都需要配置FrameStart帧,先配置Slave的,再配置Master的?

2.  第二次触发采样,我只用FrameStart帧触发Master,Slave并没有响应,按照理解Slave配置为硬触发后,应该就由SYNC_IN触发采样了,通过示波器可以确定SYNC_IN都是有信号输出的,为一个20ns的高电平脉冲;其来源是通过Master的SYNC_OUT输出的;

3. 我希望的功能是连续多次触发单次采样,但是不想每次都对所有slave 的AWR2243配置一次FrameStart帧,请问我应该如何操作?