在使用时,我是否可以用桶形插孔(中心正极)的 5V、3A 电源块,我看文档中说的是“带有 2.1mm 桶形插孔(中心正极)的 5V、> 2.5A 电源块”,但是有些人用的是5V、2A 电源块.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
在使用时,我是否可以用桶形插孔(中心正极)的 5V、3A 电源块,我看文档中说的是“带有 2.1mm 桶形插孔(中心正极)的 5V、> 2.5A 电源块”,但是有些人用的是5V、2A 电源块.
我是否可以用桶形插孔(中心正极)的 5V、3A 电源块
可以,AWR1642BOOST对板子的电源要求是 5V/>2.5A。
NOTE: A 5-V, > 2.5-A supply brick with a 2.1-mm barrel jack (center positive) is not included. TI recommends using an external power supply that complies with applicable regional safety standards, such as UL, CSA, VDE, CCC, PSE, and more. The length of the power cable should be < 3 m.