This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AWR2944EVM: mmw DDM demo BSS不启动

Part Number: AWR2944EVM
Other Parts Discussed in Thread: AWR2944

AWR2944EVM在运行mmw DDM的demo时,qspi flash启动会卡在SOC_rcmWaitBSSBootComplete()函数,好像是BSS没有启动,不知道是什么情况,串口启动信息如下所示:

Starting QSPI Bootloader ...

[09:56:49.246]收←◆[BOOTLOADER_PROFILE] Boot Media : NOR SPI FLASH
[BOOTLOADER_PROFILE] Boot Media Clock : 80.000 MHz
[BOOTLOADER_PROFILE] Boot Image Size : 77 KB
[BOOTLOADER_PROFILE] Cores present :
unknown
c66ss0
r5f0-0
[BOOTLOADER PROFILE] System_init : 132us
[BOOTLOADER PROFILE] Drivers_open : 26us
[BOOTLOADER PROFILE] Board_driversOpen : 2739us
[BOOTLOADER PROFILE] CPU load : 93197us
[BOOTLOADER_PROFILE] SBL Total Time Taken : 96097us

Image loading done, switching to application ...
INFO: Bootloader_runCpu:155: CPU r4 is initialized to 200000000 Hz !!!
INFO: Bootloader_runCpu:155: CPU c66ss0 is initialized to 360000000 Hz !!!