This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

IWR1443: The circuit output waveform is unstable at low temperatures, such as minus 35°

Part Number: IWR1443


Put the circuit board in the refrigerator at -35 degrees, the output waveform is unstable, and it will return to normal waveform after one or two minutes at room temperature.