This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LDC1612: LDC1612

Part Number: LDC1612

你好!!!

    我在使用自己搭建的LDC1612模块测量线圈到导体的距离时,出现了一些奇怪现象!!!

    测试条件:

    参考时钟20MHz,使用固定电流配置。

    测量距离大概0mm-10mm左右。(0.2mm步进)在0-2.4mm的时候数据结果很正常,随着线圈远离导体计数值减小,频率减小,电感增大。当距离为2.6mm时,计数值只出现三种结果17318412、17318417和17318421(这是不应该的,而且这种情况会一直持续,此时插入金属可以引起计数值变化,但是移开后会回复原样),同时在2.6mm正负0.1mm左右,这个输出计数值不会发生变化,依然输出这三个计数值。当距离达到2.7-2.8mm之后,计数值开始出现变化,随着线圈远离导体计数值减小,频率减小,电感增大。同时2.8mm到2.6mm的计数值变化相比2.4-2.6和2.8-3.0都要小。

    我使用过网络分析仪测量过线圈的自谐振频率大概2.5MHz左右,我选择的工作频率大概1.3MHz左右。

    下图为线圈位移过程计数值曲线。从0mm开始,逐渐远离导体,0.2mm步进,最远端为10mm。所以图中共有51个阶梯,其中2.8mm处阶梯很奇怪。

     同样的测试条件下(相同线圈和LDC1612 步进0.2mm),还可能出现另一种情况。在大致的位置,会出现步进之间计数值变化突然增大的情况,而且计数值也是只出现三种结果17318412、17318417和17318421。

    

    最后,我制作了3个相似的模块,他们在测量位移时,总会出现中间某个段计数值变化增大,而不是随着远离导体计数值的变化率逐渐减小,就如同上述第二幅图中的情况一样。

    对此我感到十分疑惑,希望能得到解答,谢谢任何人的回复。