This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

IWR1843BOOST: 如何把一帧中的chirp数减少到1,并提升慢采样频率?

Part Number: IWR1843BOOST
Other Parts Discussed in Thread: IWR1843

我使用IWR1843和DCA1000采集数据,通过UART初始化雷达并配置相应参数(cfg文件),并通过以太网端口传输原始数据到我的电脑上解析。

我的目标是一帧只采集一个chirp,当我设置一帧中的chirp数小于16时,启动雷达就不会采集数据,请问这如何解决?

如果设置好了一帧一个chirp,我还想将一帧的时间设置为0.1ms左右,如果做不到,我们雷达一帧的最低周期是多少?

谢谢

  • 我的目标是一帧只采集一个chirp,当我设置一帧中的chirp数小于16时,启动雷达就不会采集数据,请问这如何解决?

    可能是因为雷达的配置中存在某些限制,需要检查配置文件中的相关参数,确保正确设置了一帧只采集一个 chirp,并且没有其他限制导致雷达不采集数据。

    如果设置好了一帧一个chirp,我还想将一帧的时间设置为0.1ms左右,如果做不到,我们雷达一帧的最低周期是多少?

    你需要根据雷达的工作频率、chirp 个数和 chirp 间隔进行计算。一般来说,如果你的 chirp 间隔为 10us,那么 16 个 chirp 的时间就是 160us。如果你需要更短的一帧时间,可能需要调整雷达的工作频率