This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

IWR6843: 我想使用IWR6843编写心跳检测的内容,请问要参考哪个demo?

Part Number: IWR6843


我在Radar Toolbox/Example Project/Medical 中没有看到可参考的文件,里面的User Guide中提到:
Octagonal sign Before Continuing!
No Source Code Provided
This lab is provided as a binary file without source code. This can be used to test the application in various different use cases. For more information on the source code and implementation, please reach out to your local TI sales representative.

但在贴子中我看到有IWR6843的vital sign DEMO,请问这个DEMO是在开箱DEMO吗,
IWR1843BOOST: 我想使用iwr1843boost编写心跳检测的内容,请问赢参考哪个demo? - 传感器论坛 - 传感器 - E2ETm 设计支持 (ti.com)
在这个