This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AWR1843BOOST: 用DCA1000采集数据配置2个TX和4个RX的数据问题

Part Number: AWR1843BOOST

工程师你们好,我一直有一个困惑:假如我按以下配置:

ADC Samples : 128

Loops : 255

TX:2

RX:4

Frame:1

那么我最后得到的mat文件数据中,应该是4 X 65280(2X128X255)个数据 还是 4 X 32640(128X255)个数据,我看(swra581b)这个文档的介绍中似乎并没有关于多个发射天线的数据排布介绍,而且2个TX对于数据采集时,是一个发射天线将当前chirp的采样点数采集完,另一个发射天线再采集当前chirp的点数一次,即一个chirp两个发射天线分别发射采集数据一次(loop数不变),还是TX1发射当前chirp,数据采集后,TX2发射另一个chirp(loop数加1)呢?