This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

IWR1642BOOST: 雷达配置文件中的peakGrouping

Part Number: IWR1642BOOST


现在我想通过修改配置文件来生成不同的点云数据,但是配置文件中peakgrouping这个指令不太懂

有几个问题:
1:这个算法是如何实现的?我主要想了解这个算法的实现过程。(文档上说是通过输出每一帧最高峰值的点,以减少每帧点的数量,如果是这样,我该如何将没有分组之前的点输出,手动筛选峰值最高的点?)
2:是对每一帧点云单独进行峰分组,还是对所有帧的累积点云进行峰分组?
3:当我将peakGrouping -1 1 0 0 1 511修改为peakGrouping -1 1 1 1 1 511时,手上只有一个目标点。这是怎么实现的?
4:如何关闭peakGrouping?不进行峰值分组,直接将CFAR之后的所有点全部输出。
下面是我的配置文件:

sensorStop
flushCfg
dfeDataOutputMode 1
channelCfg 15 3 0
adcCfg 2 1
adcbufCfg -1 0 0 1 0
profileCfg 0 77 7 7 200 0 0 20 1 384 2000 0 0 30
chirpCfg 0 0 0 0 0 0 0 1
chirpCfg 1 1 0 0 0 0 0 2
frameCfg 0 1 16 0 100 1 0
lowPower 0 1
guiMonitor -1 1 0 0 0 0 0
cfarCfg -1 0 0 8 4 4 0 8534
cfarCfg -1 1 0 4 2 3 0 8534
peakGrouping -1 1 0 0 1 511
multiObjBeamForming -1 1 0.5
clutterRemoval -1 1
calibDcRangeSig -1 0 -5 8 256
extendedMaxVelocity -1 0
bpmCfg -1 0 0 1
lvdsStreamCfg -1 0 0 0
nearFieldCfg -1 0 0 0
compRangeBiasAndRxChanPhase 0.0 1 0 1 0 1 0 1 0 1 0 1 0 1 0 1 0
measureRangeBiasAndRxChanPhase 0 1.5 0.2
CQRxSatMonitor 0 3 19 127 0
CQSigImgMonitor 0 127 6
analogMonitor 1 1
sensorStart

非常期待大家的解惑。