I have seen the SPEC of TDC7200 and there is one thing that I can’t understand about Resolution: How is the value of 55ps get ?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
I have seen the SPEC of TDC7200 and there is one thing that I can’t understand about Resolution: How is the value of 55ps get ?
是的,就像ADC器件的分辨率,只是ADC是电压转数字信号,而TDC7200是时间转数字信号,分辨率1LSB=55ps。
是的,或者说TDC7200可以识别的最小的时间间隔为55ps。
那有TDC7200的實際量測誤差值大概會落在多少 ps 呢?
這代表的意思是, 如果我實際距離100ps,量測出來可能會落在 65ps ~ 135ps ,

我有嘗試在訊號產生器上輸入頻率1ms的訊號,但實際測試到的TOF值浮動都在 3ps~5ps之間 ,這樣是正常的嗎,感覺沒有到35ps那麼大
您好,抱歉我这边无法复制现象,大于500ns的测试推荐采用mode2,但是mode2的标准偏差典型值为35ps左右,没有最小值,所以实际测试偏差3~5ps不能判断是不是正常
我看数据手册有给出小于500ns的测试使用mode1时的标准偏差曲线,可以尝试再测试下小于500ns的信号,看是否和这个曲线的偏差是相符的。

我剛剛看一下 TDC7200的手冊 裡面是不是沒有 mode2 的 標準偏差曲線 如果有的話 可否提供呢
您好,确实没有mode 2模式下的偏差曲线。
但是偏差我们知道和输入源的精度有很大关系,数据手册给出的35ps是使用精度非常高的low jitter的脉冲发生器作为输入测试得到的结果。
您看下这个帖子,使用TDC7200 EVM测试的结果如下:可以看到比数据手册上的偏差大,可能是因为示波器探头增加了电容的原因。所以您测试得到的3~5ps偏差应该是不正常的。
| Input Interval (ns) | 12 | 50 | 100 | 200 | 500 | 1000 | 1500 |
| Measured Result (ns) | 12.49 | 50.45 | 100.45 | 200.3 | 500.29 | 1000.14 | 1500.10 |
| offset (ps) | 490 | 450 | 450 | 300 | 290 | 140 | 100 |