This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AWR1642BOOST: JTAG移入指令功能和ICEPICK_M指令的功能

Part Number: AWR1642BOOST

问题1:在JTAG中的ICEPICK_M关于此TAP的4位指令寄存器,4位指令的功能是什么,比如4‘hA,4‘hB,4‘hC,4‘hD,4‘hE,4‘hF分别对应什么功能?

问题2:在JTAG中移入指令寄存器中的42位数据,对应移出来的数据是反馈CPU的内核的 状态吗?

  • 4‘hA:模式的激活和进入

    4‘hB:模式的退出

    4‘hC:读取状态寄存器

    4‘hD:写入配置寄存器

    4‘hE:启动测试向量操作

    4‘hF:停止测试向量操作

    在JTAG中移入指令寄存器中的42位数据,对应移出来的数据是反馈CPU的内核的 状态吗?

    42位数据是用于控制和配置,不是直接反馈CPU内核状态

  • 非常感谢您的回答!我还有一些问题需要请教您。

    问题1:其他4位指令是什么功能;比如4'h1~4'h9代代表什么功能?

    问题2:什么条件转换到12位指令寄存器模式?

    问题3:您上次回答说:“4‘hD:写入配置寄存器”。我查阅了相关手册,如上图。我认为4'hD是不是读取IDCODE,您的回答是否有误?

    问题4:请问能否提供ICEPICK_M的手册资料?

  • 您好,新的问题烦请重新起帖,方便别的客户浏览,感谢理解,谢谢!