This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AWR2944: LVDS引起的死机问题

Part Number: AWR2944
Other Parts Discussed in Thread: AM2732

各位好!

       2944平台,我在配置了两个profile,进行长短波的切换的功能。配置参数如下,两个frame的切换周期是66ms:

      在实际测试时,发现2944出现随机性的死机,可能跑几百帧或者几千帧后死机。死机位置是LVDS的HW通道没有完成,如下:

定位问题时,发现DSS已经将该frame的数据处理完毕了,MSS在解析点云后,开始配置的下一帧的LVDS传输时,判断LVDS的当前活跃通道非NULL,

发现是HW的frameDoneCallbackFxn回调没有执行,所以没有将该通道close掉。即上一个frame的传输没有完成。

      请问这种问题可能是什么原因引起的?

     另外,在mmWave-Radar-Interface-Control.pdf文档里的高级chirp时间限制26us,高级chirp时间低于这个时间会有什么问题吗?