Dear TI Community Members,
I am attempting to recreate a development board circuit based on the MMWCAS-DSP-EVM board circuit, using the TDA2X chip. The configuration currently in use is the tda2xx_cascade_linux_radar version. When I connect the development board to the computer, the serial port displays that the kernel is not loading.
U-Boot SPL 2016.05-00018-g6bc25a5 (Aug 05 2019 - 14:43:03) DRA752-GP ES2.0 no pinctrl for hs200_1_8v no pinctrl for ddr_1_8v Card did not respond to voltage select! *** Warning - MMC init failed, using default environment Trying to boot from MMC1 reading dra7-ipu2-fw.lzop spl_load_file_fat: error reading file dra7-ipu2-fw.lzop, err - -1 spl: error reading image dra7-ipu2-fw.lzop, err - -1 Error loading remotecore IPU2!,Continuing with boot ... reading dra7-dsp1-fw.lzop spl_load_file_fat: error reading file dra7-dsp1-fw.lzop, err - -1 spl: error reading image dra7-dsp1-fw.lzop, err - -1 Error loading remotecore DSP1!,Continuing with boot ... reading dra7-dsp2-fw.lzop spl_load_file_fat: error reading file dra7-dsp2-fw.lzop, err - -1 spl: error reading image dra7-dsp2-fw.lzop, err - -1 Error loading remotecore DSP2!,Continuing with boot ... reading dra7-ipu1-fw.lzop spl_load_file_fat: error reading file dra7-ipu1-fw.lzop, err - -1 spl: error reading image dra7-ipu1-fw.lzop, err - -1 Error loading remotecore IPU1!,Continuing with boot ... Card did not respond to voltage select! *** Warning - MMC init failed, using default environment reading u-boot.img reading u-boot.img reading u-boot.img reading u-boot.img U-Boot 2016.05-00018-g6bc25a5 (Aug 05 2019 - 14:43:03 +0530) CPU : DRA752-GP ES2.0 Model: TI DRA742 Board: DRA74x EVM REV DRAM: 1.5 GiB MMC: i2c_write: error waiting for data ACK (status=0x116) pcf8575_i2c_write_le16 i2c write failed to addr 21 OMAP SD/MMC: 0, OMAP SD/MMC: 1 Card did not respond to voltage select! *** Warning - MMC init failed, using default environment Warning: fastboot.board_rev: unknown board revision Card did not respond to voltage select! ERROR: invalid mmc device at arch/arm/cpu/armv7/omap-common/utils.c:193/mmc_get_part_size() Warning: fastboot.userdata_size: unable to calc SCSI: SATA link 0 timeout. AHCI 0001.0300 32 slots 1 ports 3 Gbps 0x1 impl SATA mode flags: 64bit ncq stag pm led clo only pmp pio slum part ccc apst scanning bus for devices... Found 0 device(s). Net: Could not get PHY for ethernet@48484000: addr 2 Warning: ethernet@48484000 using MAC address from ROM eth0: ethernet@48484000 Hit any key to stop autoboot: 0 ## Error: "board_findfdt" not defined MMC: no card present MMC: no card present MMC: no card present Card did not respond to voltage select! MMC: no card present Card did not respond to voltage select! ** Bad device mmc 1 ** Card did not respond to voltage select! ** Bad device mmc 1 ** Card did not respond to voltage select! ** Bad device mmc 1 ** Card did not respond to voltage select! ** Bad device mmc 1 ** mmc - MMC sub system Usage: mmc info - display info of the current MMC device mmc read addr blk# cnt mmc write addr blk# cnt mmc erase blk# cnt mmc rescan mmc part - lists available partition on current mmc device mmc dev [dev] [part] - show or set current mmc device [partition] mmc list - lists available devices mmc hwpartition [args...] - does hardware partitioning arguments (sizes in 512-byte blocks): [user [enh start cnt] [wrrel {on|off}]] - sets user data area attributes [gp1|gp2|gp3|gp4 cnt [enh] [wrrel {on|off}]] - general purpose partition [check|set|complete] - mode, complete set partitioning completed WARNING: Partitioning is a write-once setting once it is set to complete. Power cycling is required to initialize partitions after set to complete. mmc bootbus dev boot_bus_width reset_boot_bus_width boot_mode - Set the BOOT_BUS_WIDTH field of the specified device mmc bootpart-resize <dev> <boot part size MB> <RPMB part size MB> - Change sizes of boot and RPMB partitions of specified device mmc partconf dev boot_ack boot_partition partition_access - Change the bits of the PARTITION_CONFIG field of the specified device mmc rst-function dev value - Change the RST_n_FUNCTION field of the specified device WARNING: This is a write-once field and 0 / 1 / 2 are the only valid values. mmc setdsr <value> - set DSR register value mmc - MMC sub system Usage: mmc info - display info of the current MMC device mmc read addr blk# cnt mmc write addr blk# cnt mmc erase blk# cnt mmc rescan mmc part - lists available partition on current mmc device mmc dev [dev] [part] - show or set current mmc device [partition] mmc list - lists available devices mmc hwpartition [args...] - does hardware partitioning arguments (sizes in 512-byte blocks): [user [enh start cnt] [wrrel {on|off}]] - sets user data area attributes [gp1|gp2|gp3|gp4 cnt [enh] [wrrel {on|off}]] - general purpose partition [check|set|complete] - mode, complete set partitioning completed WARNING: Partitioning is a write-once setting once it is set to complete. Power cycling is required to initialize partitions after set to complete. mmc bootbus dev boot_bus_width reset_boot_bus_width boot_mode - Set the BOOT_BUS_WIDTH field of the specified device mmc bootpart-resize <dev> <boot part size MB> <RPMB part size MB> - Change sizes of boot and RPMB partitions of specified device mmc partconf dev boot_ack boot_partition partition_access - Change the bits of the PARTITION_CONFIG field of the specified device mmc rst-function dev value - Change the RST_n_FUNCTION field of the specified device WARNING: This is a write-once field and 0 / 1 / 2 are the only valid values. mmc setdsr <value> - set DSR register value Booting from eMMC ... Wrong Image Format for bootm command ERROR: can't get kernel image!
The image below is a comparison of the serial output from my custom board and the MMWCAS-DSP-EVM output. Could you advise on how to modify the configuration files to enable the system to boot properly? Is it necessary to flash the onboard EEPROM?
Thank you for any assistance or guidance on relevant documentation.