This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AWR2243: AWR2243配置问题

Part Number: AWR2243
Other Parts Discussed in Thread: , UNIFLASH

您好,工程师!

我最近在使用AWR2243这款毫米波芯片做开发,在如何配置芯片方面遇到了一些问题。由于官方的AWR2243Boost评估板太大,我们自行设计了一款子板,且使用的flash等芯片均与评估板保持一致。请问以这种设计能否实现使用usb接到电脑上用mmwave studio配置参数,并且固化到flash,并实现AWR2243上电启动通过flash加载参数。主要担心我们这样设计的子板能否被MMWWAVE Studio和Uniflash正常识别到,并能够实现参数配置以及参数固化到flash的功能。请您帮我们解答一下,谢谢!

Hello, engineer!


I have been using the AWR2243 millimeter wave chip for development recently and have encountered some issues on how to configure the chip. Due to the official AWR2243Boost evaluation board being too large, we have designed a sub board ourselves and used chips such as flash that are consistent with the evaluation board. May I ask if this design can enable the use of USB to connect to a computer and configure parameters using mmwave studio, and solidify them into flash, and enable AWR2243 to power on and load parameters through flash. The main concern is whether our designed sub board can be recognized by MMWWAVE Studio and Uniflash, and can achieve parameter configuration and parameter solidification to flash. Could you please help us answer this question? Thank you!

  • Hello Rovine,

    The main concern

    Understand your concerns.
    In terms of hardware, you need to ensure that the USB interface on the sub board can be correctly recognized when connected to the computer, and has a high similarity to the hardware configuration of the evaluation board, including the model and interface of the Flash chip. In addition, ensuring the stability and correctness of key components such as power supply and clock is also crucial.
    In terms of software, the key to ensuring that your daughter board can communicate with MMWave Studio and Uniflash is to correctly configure the communication protocol.

    Happy New Year,

    Gary