Other Parts Discussed in Thread: MMWAVEICBOOST, IWR6843AOPEVM, , IWR6843ISK-ODS
我有关注到IWR6843AOPEVM的原始ADC数据采集需要mmwaveICBOOST,请问AWR6843AOPEVM也需要mmwaveICBOOST来采集原始ADC数据吗,mmwaveICBOOST的作用是什么?只用DCA1000会得到什么

This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
我有关注到IWR6843AOPEVM的原始ADC数据采集需要mmwaveICBOOST,请问AWR6843AOPEVM也需要mmwaveICBOOST来采集原始ADC数据吗,mmwaveICBOOST的作用是什么?只用DCA1000会得到什么

感谢您对TI产品的关注!
关于你的咨询,IWR6843AOPEVM 不支持直接和DCA1000配合。
而xWR6843ISK和IWR6843ISK-ODS,支持和DCA1000直接配合。

mmWaveICBOOST你可以把它看作一个扩展接口的底座。
下面是它的功能。
1.2.5 MMWAVEICBOOST
• Hosts starter kit using two 60-pin high-density (HD) connector for the high-speed ADC data over CSI or LVDS
and emulator signals
• FTDI-based JTAG emulation with serial port for programming flash on the starter kit
• XDS110-UART based QSPI flash programming
• 60-pin HD connector to interface with the DCA1000 EVM
• Two 20-pin LaunchPad connectors that leverage the ecosystem of the TI standard Launchpad and have all of
the digital controls from the Radar chip
• Two onboard controller area network (CAN) transceivers
• On-board PMIC
• 60-pin MIPI HD connector for JTAG trace
• On-board FTDI chip to provide PC interface for serial peripheral interface (SPI), general-purpose input/output
(GPIO) controls and universal asynchronous receiver/transmitter (UART) loggers
• On-board current sensors and temperature sensors
希望对你有所帮助。