This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TDC1011: TDC1011PGA输出

Part Number: TDC1011


TDC1011PGA输出的回波信号频移的准确性怎么样,可不可以以此回波信号作为多普勒信号处理

  • TDC1011PGA是一款高精度的时间数字转换器(TDC),应用于距离测量、速度测量等场景,其中也包括基于回波信号的多普勒效应测量。

    关于TDC1011PGA输出的回波信号频移的准确性,它主要取决于硬件特性,环境因素,以及信号处理。

    比如, 该芯片的时间分辨率和测量精度是其基本性能参数,这些参数将直接影响回波信号频移的测量准确性。
    滤波、放大、降噪等回波信号的处理步骤都可能影响信号的完整性和准确性。
    噪声、温度变化、电磁干扰等因素也可能对回波信号的频移测量产生影响。

    因此,如果你考虑使用TDC1011PGA进行多普勒信号处理,最近进行充分的测试测量和验证,以判断其能否满足你的应用需求。