This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AWR1642BOOST: AWR1642BOOST

Part Number: AWR1642BOOST


请问我用以下的配置参数:Scene Classifier:best_vel_res Azimuth Resolution(deg):15 Range Resolution(m):0.178 Maximum unambiguous Range(m):9.11 Maximum Radial Velocity(m/s):2.56 Radial velocity resolution(m/s):0.04 Frame Duration(msec):100 RF calibration data:None Range Detection Threshold (dB):15 Doppler Detection Threshold (dB):15 Range Peak Grouping:enabled Doppler Peak Grouping:enabled Static clutter removal:disabled Angle of Arrival FoV: Full FoV Range FoV: Full FoV 请问AWR1642BOOST的点云辐射范围有多少? 能具体到长和宽吗?