ar1.ChanNAdcConfig_mult 不明白,我找了许久,没有明白ar1.ChanNAdcConfig_mult(1,1,1,1, 1,1,1,1, 2,1,0,1)语句中的(1,1,1,1, 1,1,1,1, 2,1,0,1)具体表示什么意思呢?-- Channel & ADC Configuration
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
ar1.ChanNAdcConfig_mult 不明白,我找了许久,没有明白ar1.ChanNAdcConfig_mult(1,1,1,1, 1,1,1,1, 2,1,0,1)语句中的(1,1,1,1, 1,1,1,1, 2,1,0,1)具体表示什么意思呢?Hi
可在studio 中的LUA shell 中输入help 查看
>help ar1.ChanNAdcConfig_mult
Int32 ar1.ChanNAdcConfig_mult(UInt16 RadarDeviceId, UInt16 Tx0En, UInt16 Tx1En, UInt16 Tx2En, UInt16 Rx0En, UInt16 Rx1En, UInt16 Rx2En, UInt32 Rx3En, Int32 BitsVal, UInt32 FmtVal, UInt32 IQSwap, UInt16 CasCadeMode) - Static device config API which defines configure both the Transmiter and Reciever channels of Radar device and also ADC data format output
_I_ UInt16 RadarDeviceId - Radar Device Id
_I_ UInt16 Tx0En - Tx0 channel
_I_ UInt16 Tx1En - Tx1 channel
_I_ UInt16 Tx2En - Tx2 channel
_I_ UInt16 Rx0En - Rx0 channel
_I_ UInt16 Rx1En - Rx1 channnel
_I_ UInt16 Rx2En - Rx2 channel
_I_ UInt32 Rx3En - Rx3 channel[b15:0] + (CascadePinOutCfg[b31:16] b16:ClkOutMasterDis, b17:SynOutMasterDis, b18:ClkOutSlaveEna, b19:SynOutSlaveEna, b20:IntLOMasterEna, b21:OSCClkOutMasterDis)
_I_ Int32 BitsVal - Number of ADC bits
_I_ UInt32 FmtVal - ADC output format[b15:0] + FullScaleReductionFactor[b31:16]
_I_ UInt32 IQSwap - ADC Mode
_I_ UInt16 CasCadeMode - CascadeMode(Single Chip: 0x0000, MultiChip Master:0x0001, MultiChip Slave:0x0002)
Thanks
Ken
您能继续帮看看这两个问题怎么回事吗?如何改错。
Q1:AWR2243: 自定义修改Cascade_Configuration_MIMO.lua后出错!