你好!
由于使用IWR6843芯片设计的产品在测试时能检测到活物的距离只有2米远,请问能有什么方法测试出芯片的输出功率是否正常。

This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
你好,
芯片内部发TX发送功率,可以通过监控模块监控。你可以参考\mmwave_sdk_03_06_00_00-LTS\packages\ti\demo\utils\mmwdemo_monitor.c里mmwDemo_cfgAnalogMonitor,使能TX power的监控。
mmwdemo_monitor.h
typedef enum mmwDemo_AnaMonitor_e
{
MMWDEMO_ANALOG_MONITOR_TEMPERATURE = 0U,
MMWDEMO_ANALOG_MONITOR_RX_GAIN_PHASE,
MMWDEMO_ANALOG_MONITOR_RX_NOISE_FIGURE,
MMWDEMO_ANALOG_MONITOR_IFSTAGE,
MMWDEMO_ANALOG_MONITOR_TX0_POWER,
MMWDEMO_ANALOG_MONITOR_TX1_POWER,
MMWDEMO_ANALOG_MONITOR_TX2_POWER,
MMWDEMO_ANALOG_MONITOR_TX0_BALLBREAK,
MMWDEMO_ANALOG_MONITOR_TX1_BALLBREAK,
MMWDEMO_ANALOG_MONITOR_TX2_BALLBREAK,
MMWDEMO_ANALOG_MONITOR_TX_GAIN_PHASE_MISMATCH,
MMWDEMO_ANALOG_MONITOR_TX0_BPM,
MMWDEMO_ANALOG_MONITOR_TX1_BPM,
MMWDEMO_ANALOG_MONITOR_TX2_BPM,
MMWDEMO_ANALOG_MONITOR_SYNTH_FREQ,
MMWDEMO_ANALOG_MONITOR_EXT_ANALOG_SIGNALS,
MMWDEMO_ANALOG_MONITOR_INTERNAL_TX0_SIGNALS,
MMWDEMO_ANALOG_MONITOR_INTERNAL_TX1_SIGNALS,
MMWDEMO_ANALOG_MONITOR_INTERNAL_TX2_SIGNALS,
MMWDEMO_ANALOG_MONITOR_INTERNAL_RX_SIGNALS,
MMWDEMO_ANALOG_MONITOR_INTERNAL_PMCLKLO_SIGNALS,
MMWDEMO_ANALOG_MONITOR_INTERNAL_GPADC_SIGNALS,
MMWDEMO_ANALOG_MONITOR_PLL_CONTROL_VOLTAGE,
MMWDEMO_ANALOG_MONITOR_DCC_CLOCK_FREQ,
MMWDEMO_ANALOG_MONITOR_RX_SATURATION_DETECTOR,
MMWDEMO_ANALOG_MONITOR_RX_SIG_IMG_BAND,
MMWDEMO_ANALOG_MONITOR_RX_MIXER_INPUT_POWER,
MMWDEMO_ANALOG_MONITOR_MAX
}mmwDemo_AnaMonitor;
Thanks,
Chris