This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AWR2243: 虚拟阵列

Part Number: AWR2243


请问对于远场窄带静止目标来说,由2发4收的实际天线虚拟成的1发8收的天线,这个时候的1发8收的虚拟接收天线接收到的信号X1和实际物理1发8收的物理接收天线接收到的信号X2会一模一样吗?我要是拿接收信号X2和 X1做DOA估计会有区别吗? 如果我想让【2发4收的实际物理天线-->1发8收的虚拟接收天线】实际效果完全等于【1发8收的实际物理天线】,怎么做能实现?

  • 对于远场窄带静止目标来说,由2发4收的实际天线虚拟成的1发8收的天线阵列接收到的信号(X1)和实际物理1发8收的天线阵列接收到的信号(X2)不会完全一模一样。虚拟天线阵列由于时分复用引入的时间差和相位修正,接收到的信号可能存在一些细微差别。因此,使用接收信号X2和X1进行DOA估计时,结果可能会有一定的区别。实际物理天线阵列的DOA估计通常会更为准确和可靠。

    为了消除时间差(这里是指的不同发射天线的chirpj间隔?),我让TX0 TX1同时发射chirp,请问我在mmwave3.0.14使用GUI进行如下两张图所示这样的设置,请问可行吗?能实现不?

  •  天线同时发射应该是属于DDM体制吧。这个体制下为了不混淆每个发射天线的数据,会将每个发射天线的信号都偏移一个特定的频率。我现在想混淆他们,比如将两根发射天线TX0 TX1当作一个根发射天线可以吗(即将2发4收物理天线的效果=1发8收物理天线)?

  • 你好

    通过TDM模式实现的MIMO雷达在性能上无法完全等同于对应的实孔径雷达。你可以通过TDM或者DDM等方法进行接收通道的分离,进而获得虚拟阵列。DDM模式的具体工作原理建议你阅读如下文档:

    ti.com.cn/cn/lit/an/zhcab85/zhcab85.pdf?ts=1715947233933&ref_url=https%253A%252F%252Fwww.ti.com.cn%252Fproduct%252Fcn%252FAWR2944