This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

HDC1080: 芯片的应用问题

Part Number: HDC1080

我司在开发一款项目,项目名称:酒精连锁装置,年用量:预计700k.

选用了TI的温湿度传感器,型号: HDC1080DMBR DFN-6(3x3)

目前遇到以下问题:

HDC1080,通信建立成功之后。只能读取设备ID号,读取不到温湿度值,为空,默认为零.

请帮忙看一下哪里有问题,应该怎么解决?谢谢!

以下是原理图和软件供参考

#include "dmm_hdc1080.h"
#include "dmm_function.h"
#include "dmm_gpio.h"
#include "dmm_systick.h"
#include "dmm_timer_module.h"
#include "math.h"
//******************************************************************************************//
#define  IIC_DELAY		50
//******************************************************************************************//
static void iic_start(void)
{
		SDA_OUT_H;	delay_us(IIC_DELAY);
		SCL_OUT_H;	delay_us(IIC_DELAY);
		SDA_OUT_L;	delay_us(IIC_DELAY);
		SCL_OUT_L;	delay_us(IIC_DELAY);
}
//******************************************************************************************//
static void iic_stop(void)
{
		SCL_OUT_L;	delay_us(IIC_DELAY);
		SDA_OUT_L;	delay_us(IIC_DELAY);
		SCL_OUT_H;	delay_us(IIC_DELAY);
		SDA_OUT_H;	delay_us(IIC_DELAY);
}
//******************************************************************************************//
static uint8 iic_wait_ack(void)
{
		uint8 ERROR_TIME=0;
		SDA_OUT_H;	delay_us(IIC_DELAY);
		SCL_OUT_H;	delay_us(IIC_DELAY);
		while(SDA_IN)
		{
				ERROR_TIME++;
				if(ERROR_TIME>250)	{iic_stop();return 1;}
		}
		SCL_OUT_L;	delay_us(IIC_DELAY);
		return 0;
}
//******************************************************************************************//
static void iic_ack(void)
{
		SCL_OUT_L;	delay_us(IIC_DELAY);
		SDA_OUT_L;	delay_us(IIC_DELAY);
		SCL_OUT_H;	delay_us(IIC_DELAY);
		SCL_OUT_L;	delay_us(IIC_DELAY);
}
//******************************************************************************************//
static void iic_no_ack(void)
{
		SCL_OUT_L;	delay_us(IIC_DELAY);
		SDA_OUT_H;	delay_us(IIC_DELAY);
		SCL_OUT_H;	delay_us(IIC_DELAY);
		SCL_OUT_L;	delay_us(IIC_DELAY);
}
//******************************************************************************************//
static void iic_send_byte(uint8 txd)
{
    uint8 t;
    SCL_OUT_L;delay_us(IIC_DELAY);
    for(t=0;t<8;t++)
    {
				if((txd&0x80)>>7)		SDA_OUT_H;
				else								SDA_OUT_L;
				txd<<=1;						delay_us(IIC_DELAY);
				SCL_OUT_H;					delay_us(IIC_DELAY);
				SCL_OUT_L;					delay_us(IIC_DELAY);
    }
}
//******************************************************************************************//
static uint8 iic_read_byte(uint8 ack)
{
    uint8 i,receive=0;
    SDA_OUT_H;delay_us(IIC_DELAY);
    for(i=0;i<8;i++ )
    {
        SCL_OUT_L;						delay_us(IIC_DELAY);
				SCL_OUT_H;						delay_us(IIC_DELAY);
				receive<<=1;
        if(SDA_IN)						receive++;
    }
    if(!ack)							iic_no_ack();
    else									iic_ack();
    return receive;
}
//******************************************************************************************//
extern void HDC1080_Write_Register(u8 Addr,u16 Data)
{
		unsigned char data[2];
		data[0] = (uint8_t)((Data& 0xFF00) >> 8); 			//¸ß°ËλÊý¾Ý
		data[1] = (uint8_t)(Data & 0x00FF); 						//µÍ°ËλÊý¾Ý
		iic_start();
		iic_send_byte(HDC1080_WRITE_ADDR);iic_wait_ack(); //µØÖ·Îª10000000£¬Ð´¼Ä´æÆ÷
		iic_send_byte(Addr);iic_wait_ack(); //д¼Ä´æÆ÷µØÖ·
		iic_send_byte(data[0]);iic_wait_ack(); //·¢Ë͸߰ËλÊý¾Ý
		iic_send_byte(data[1]);iic_wait_ack(); //·¢Ë͵ͰËλÊý¾Ý
		iic_stop(); //Í£Ö¹ÐźÅ
}
//******************************************************************************************//
unsigned char HDC1080_Read_Register(unsigned char ReadAddr,unsigned char *buf,unsigned int length)
{	
		uint8_t i = 0;
	            
	iic_start();   									//ÆðʼÐźÅ
	iic_send_byte(HDC1080_WRITE_ADDR);			//HDC1080É豸µØÖ·(7λÉ豸µØÖ·+W/R)
	iic_wait_ack();									//²úÉúÓ¦´ð
	iic_send_byte(ReadAddr);						//¼Ä´æÆ÷µØÖ·
	iic_wait_ack();									//²úÉúÓ¦´ð
	
	iic_start();									//ÆðʼÐźÅ
	iic_send_byte(HDC1080_READ_ADDR);			    //HDC1080É豸µØÖ·(7λÉ豸µØÖ·+W/R) ¶Á
	iic_wait_ack();									//²úÉúÓ¦´ð
	for(i = 0; i < length-1; i++)
	{
		buf[i] = iic_read_byte(1);					//¶ÁÊý¾Ý
	}
	buf[i] = iic_read_byte(0);						//¶ÁÊý¾Ý
	
	iic_stop();													//Í£Ö¹ÐźŠ 
	
	return 0;
}
//******************************************************************************************//
void Read_TH_Register(unsigned char *pbuff)
{
	uint8_t length = 4, i = 0;					    //ת»»Êý¾Ý×Ö½ÚÊý
	
	iic_start();   									//ÆðʼÐźÅ
	iic_send_byte(HDC1080_WRITE_ADDR);			//HDC1080É豸µØÖ·(7λÉ豸µØÖ·+W/R)
	iic_wait_ack();									//²úÉúÓ¦´ð
	iic_send_byte(HDC1080_TEMPERATURE_ID);		//´¥·¢Ê¼þµØÖ·
	iic_wait_ack();									//²úÉúÓ¦´ð
	iic_stop();	
	
	delay_ms(50);									//µÈ´ýת»¯
	iic_start();   									//ÆðʼÐźÅ
	iic_send_byte(HDC1080_READ_ADDR);				//HDC1080É豸µØÖ·(7λÉ豸µØÖ·+W/R) ¶Á
	iic_wait_ack();									//²úÉúÓ¦´ð
	for(i = 0; i < length-1; i++)
	{
		pbuff[i] = iic_read_byte(1);				//¶ÁÊý¾Ý
	}                        
	pbuff[i] = iic_read_byte(0);                     

	iic_stop();										//Í£Ö¹ÐźŠ  
}
//******************************************************************************************//
void HDC1080_Driver_Init(void)
{
	uint8_t menufacture_buf[2] = {0}, device_buf[2] = {0};
	uint16_t menufacture_id = 0, device_id = 0;
	
	HDC1080_Read_Register(HDC1080_MENUFACTURE_ID, menufacture_buf, 2);
	menufacture_id = (uint16_t)(menufacture_buf[0]<<8);
	menufacture_id |= menufacture_buf[1];
	
	HDC1080_Read_Register(HDC1080_DEVICE_ID, device_buf, 2);
	device_id = (uint16_t)(device_buf[0]<<8);
	device_id |= device_buf[1];
	if(menufacture_id==HDC1080_MENUFACTURE_ID_VALUE&&device_id==HDC1080_DEVICE_ID_VALUE)
	{
		printf("<-----HDC1080 Á¬½Ó³É¹¦£¡----->\r\n");
	}
	else
		printf("<-----HDC1080 Á¬½Óʧ°Ü£¡----->\r\n");   
	//ÉèÖÃͬʱ²É¼¯Î¶ȺÍʪ¶È 14λ·Ö±æÂÊ   Ö»Òª·¢ËÍÒ»¸ö´¥·¢ÃüÁîÎÂʪ¶È¾Í»áÁ¬Ðø×¼»»
	HDC1080_Write_Register(HDC1080_CONFIG_ID, HDC1080_CONFIG_VALUE);  
}
//******************************************************************************************//
void Get_HDC1080_THValue(float *temp, float *humid)
{
	uint8_t buf[4] = {0};
	
	//¶ÁÎÂʪ¶È¼Ä´æÆ÷Öµ±£´æÔÚÊý×éÖÐ
	Read_TH_Register(buf);
	//ζÈת»»
	*temp = (float)(buf[0]<<8|buf[1]);
	*temp = (*temp/pow(2,16))*165-40;
	//ʪ¶Èת»»
	*humid = (float)(buf[2]<<8|buf[3]);
	*humid = (*humid/pow(2, 16))*100;
}
//******************************************************************************************//




.h

#ifndef  _DMM_DMM_HDC1080_H_
#define  _DMM_DMM_HDC1080_H_

/******************************************************************************/ 
#include "dmm_type.h"
/******************************************************************************/   
//¼Ä´æÆ÷µØÖ·
typedef enum{
	HDC1080_WRITE_ADDR = 		0x80,
	HDC1080_READ_ADDR = 		0x81,
	HDC1080_MENUFACTURE_ID = 	0xfe,
	HDC1080_DEVICE_ID = 		0xff,
	HDC1080_CONFIG_ID = 		0x02,
	HDC1080_TEMPERATURE_ID =    0x00,
	HDC1080_HUMIDITY_ID	= 		0x01,
}REGISTER_ADDR;
 
//¼Ä´æÆ÷Öµ
typedef enum
{
	HDC1080_MENUFACTURE_ID_VALUE = 	 0x5449,
	HDC1080_DEVICE_ID_VALUE = 		 0x1050,
	HDC1080_CONFIG_VALUE = 			 0x1000,		//ÎÂ¶È Êª¶Èͬʱת»» 14λ·Ö±æÂÊ
}REGISTER_VALUE;
 
void HDC1080_Driver_Init(void);
extern void HDC1080_Write_Register(u8 Addr,u16 Data);
unsigned char HDC1080_Read_Register(unsigned char ReadAddr, unsigned char *buf, unsigned int length);
void Read_TH_Register(unsigned char *pbuff);
void Get_HDC1080_THValue(float *temp, float *humid);
/******************************************************************************/

#endif